Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84482members
353698posts

Citect Computer Setup Wizard failing.

AVEVA Plant SCADA Forum

A support forum for AVEVA Plant SCADA (formerly Citect SCADA). Share new and exciting product information, connect, learn, and collaborate with the ecosystem of Plant SCADA Users. AVEVA Plant SCADA a reliable, flexible and high-performance Supervisory Control and Data Acquisition software solution for industrial process customers. This forum is to connect, share, learn and collaborate new and exciting product information. Feel free to join and share to your Ecosystem of Plant SCADA Users.

Topher
Crewman
Crewman
7
3223

Citect Computer Setup Wizard failing.

I'm very new to Citect scada software and have installed the Citect SCADA 2018 R2 v8.2.

 

I have an issue when I run the Computer set up wizard in that it fails to store the security credentials and it cannot complete.

I cannot find any information on this problem so am hoping to find it here.

 

The attached images shows the error I receive upon completing the set up process.

 

Thanks.

Attachments
Tags (1)
7 Replies 7
Rodrigo_Garcia
Administrator Administrator
Administrator
0 Likes
3
3203

Re: Citect Computer Setup Wizard failing.

Hello @btekkiam Could you support in this, please?

 

 

Rodrigo G. 


Industrial Automation Community manager

Tags (1)
Topher
Crewman
Crewman
0 Likes
2
3185

Re: Citect Computer Setup Wizard failing.

I have managed to get by for now but it would be good to identify the cause for future reference.

I've simply disabled the computer setup check prior to running the program and it is running ok for my needs.

 

I am only using the Citect SCADA software temporarily to test the functionality of the PLC code that it is interfacing with.

For this reason, I have also not configured a System Management Server as I was having issues with ports and it was not required for my purpose.

 

Perhaps the setup wizard failing has something to do with fact that there is no System Management Server configured.

Tags (1)
btekkiam
Lieutenant JG Lieutenant JG
Lieutenant JG
1
3089

Re: Citect Computer Setup Wizard failing.

Hi @Topher Did you manage to get around this problem? I also don't have SMS configured, and I get the same error.

 

If I run %programfiles(x86)%\AVEVA\Citect SCADA 2018 R2\Bin\CtSetup.exe as administrator I don't get the error and the settings do get saved.

 

Edit: The issue is probably due to the fact that a restart is needed so that the currently logged-in user is properly assigned to the Windows groups created by the Citect installer.

Tags (1)
Topher
Crewman
Crewman
0 Likes
0
3082

Re: Citect Computer Setup Wizard failing.

Hi @btekkiam 

I got around the problem by turning off the auto check for Computer Setup in the options. After this, I was no longer prompted to run the Wizard and was able to run the program.

Not a long term fix but it was adequate for me as I only developed the SCADA interface so that I could test the function and data mapping of the PLC that it was connected to.  After that, it wasn't needed any more.

Tags (1)
NGUYENVANQUY
Cadet
0 Likes
2
2730

Re: Citect Computer Setup Wizard failing.


@Topher wrote:

I'm very new to Citect scada software and have installed the Citect SCADA 2018 R2 v8.2.

 

I have an issue when I run the Computer set up wizard in that it fails to store the security credentials and it cannot complete.

I cannot find any information on this problem so am hoping to find it here.

 

The attached images shows the error I receive upon completing the set up process.

 

Thanks.


You run Citect Studio run as administrator is fixed it.

Tags (1)
wte
Cadet
0 Likes
1
2282

Re: Citect Computer Setup Wizard failing.

Hi

 

I've been working with Citect Studio for several weeks.
When I wanted to continue working on the project this week, run-time no longer worked. Error message: "The user must have access to the server password to run as part of the trusted domain."
I then tried to do a new "Computer Setup".
New error message: Storing security credentials failed. Setup wizard cannot complete.
Attempting to run Citect Studio as an administrator did not get me there.
I'm using version 8.20 R2.
A Windows update may have been installed automatically at the end of last week.

 

Wolfgang

Tags (1)
kingslim
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
2272

Re: Citect Computer Setup Wizard failing.

I have heard of this issue before. Over here in Thailand, our SAE Jeerawat somehow resolved the issue by messing around with the Configurator. Something about re-configuring the Configurator again. 

Tags (1)