Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84829members
354283posts

possible to use apc powerchute to monitor UPS's connected via network?

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
gilly2006_apc
Crewman
Crewman
0 Likes
1
174

possible to use apc powerchute to monitor UPS's connected via network?

This was originally posted on APC forums on 7/27/2009


Hi all,
I was asked today to find out whether it was possible to monitor multiple Smart-UPS units connected to the network via 1 powerchute business edition installation. This means that the UPS are not direct attached to the server.

Also if this is possible could you also please outline the steps required for this to work.

Please ask if you require further information.

Thanks
Michael

Message was edited by: gilly2006


Accepted Solutions
Erasmus_apc
Sisko
Sisko
0 Likes
0
174

Re: possible to use apc powerchute to monitor UPS's connected via network?

This was originally posted on APC forums on 7/27/2009


This is not possible, as PCBE requires the actual "computer" to act as the agent, which then communicates with the PCBE "Server" that you have installed. PCBE requires a direct UPS-to-computer connection. PowerChute Network Shutdown does not, and allows for shutdown or other functionality all based on TCP/IP. PCNS does require network management cards in the UPS', however.

See Answer In Context

1 Reply 1
Erasmus_apc
Sisko
Sisko
0 Likes
0
175

Re: possible to use apc powerchute to monitor UPS's connected via network?

This was originally posted on APC forums on 7/27/2009


This is not possible, as PCBE requires the actual "computer" to act as the agent, which then communicates with the PCBE "Server" that you have installed. PCBE requires a direct UPS-to-computer connection. PowerChute Network Shutdown does not, and allows for shutdown or other functionality all based on TCP/IP. PCNS does require network management cards in the UPS', however.