Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84545members
353800posts

is the Universal I/O Temperature exposed via SNMP?

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Kola
Crewman
Crewman
0 Likes
3
553

is the Universal I/O Temperature exposed via SNMP?

Hi!

I have an SRT8KXLI, and wonder if i can fetch the (universal i/o) temperature via SNMP?
Also the load and battery temperature and such would be nice.

Tags (1)
3 Replies 3
BillP
Administrator Administrator
Administrator
0 Likes
2
549

Re: is the Universal I/O Temperature exposed via SNMP?

@Kola 

Yes. You can capture all of those.

 

IO.png

 

 

 

Tags (1)
Kola
Crewman
Crewman
0 Likes
1
542

Re: is the Universal I/O Temperature exposed via SNMP?

I can get the battery temp and load, thanks!  Not the probe temp though.

On the web interface i can see it though.

 

Screenshot_2021-10-26_12-57-48.pngScreenshot_2021-10-26_12-56-49.png

Attachments
Tags (1)
Kola
Crewman
Crewman
0 Likes
0
538

Re: is the Universal I/O Temperature exposed via SNMP?

It seems there are two oids for the load?

 

Screenshot_2021-10-26_13-02-25.png

Tags (1)