Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84570members
353843posts

configuring email alerting through SNMP traps

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
sp_apc
Crewman
Crewman
0 Likes
3
1004

configuring email alerting through SNMP traps

This was originally posted on APC forums on 11/11/2008


I'm working on connecting two SmartUPS 1000 and configuring them to notify us in the event of powerissues. Unfortunately, I cannot get email or pager notifications to go through because SMTP authentication is required to send mail within my company. Mail is hosted external and so all email traffic must authenticate to go through.

I don't believe that the hosting provider will make any changes, and since there is no way to setup authentication through the PowerChute software, I'm kind of stuck. I proposed setting up an SMTP or sendmail server , but my director doesn't want one internal to the company.

I called APC support and they recommended setting up an SNMP server and have that server authenticate through SMTP to send email. Has anyone done this and can they point me in the right direction?

I've configured SNMP on the server that I'm using as the APC Server, but I understand I also need to setup an SNMP server with the APC MIB, and I'm completely in the dark about that. Any assistance would be greatly appreciated!


Accepted Solutions
TheNotoriousKMP_apc
Sisko
Sisko
0 Likes
0
1004

Re: configuring email alerting through SNMP traps

This was originally posted on APC forums on 11/11/2008


So you're using SNMP to have a trap from the APC device sent to some type of NMS, which is then in turn going to send the email?

SNMP from an APC device cannot authenticate any type of email, nor even send email, it's SNMP.

To me, it doesn't seem like the combination of SNMP and an SMTP server that requires authentication is going to work, unless your NMS can authenticate.

See Answer In Context

3 Replies 3
TheNotoriousKMP_apc
Sisko
Sisko
0 Likes
0
1004

Re: configuring email alerting through SNMP traps

This was originally posted on APC forums on 11/11/2008


At this time, the firmware does not allow for coding of authentication to send email from the Network device.

sp_apc
Crewman
Crewman
0 Likes
0
1004

Re: configuring email alerting through SNMP traps

This was originally posted on APC forums on 11/11/2008


I don't know what happened, but my message got truncated. Here is the rest of it: I don't believe that the hosting provider will make any changes, and since there is no way to setup authentication through the PowerChute software, I'm kind of stuck. I proposed setting up an SMTP or sendmail server , but my director doesn't want one internal to the company. I called APC support and they recommended setting up an SNMP server and have that server authenticate through SMTP to send email. I've configured SNMP on the server that I'm using as the APC Server, but I understand I also need to setup an SNMP server with the APC MIB, and I'm completely in the dark about that. Has anyone done this and can they point me in the right direction? Any assistance would be greatly appreciated!

TheNotoriousKMP_apc
Sisko
Sisko
0 Likes
0
1005

Re: configuring email alerting through SNMP traps

This was originally posted on APC forums on 11/11/2008


So you're using SNMP to have a trap from the APC device sent to some type of NMS, which is then in turn going to send the email?

SNMP from an APC device cannot authenticate any type of email, nor even send email, it's SNMP.

To me, it doesn't seem like the combination of SNMP and an SMTP server that requires authentication is going to work, unless your NMS can authenticate.