Welcome to the new Schneider Electric Community

It's your place to connect with experts and peers, get continuous support, and share knowledge.

Close
Important Announcement: WELCOME to the Schneider Electric Community! We have moved to a new address: community.se.com — bookmark it today and contact SchneiderCommunity.Support@se.com if you have any questions!
Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
82779members
350593posts

Symmetra LX SYAF16KRMT Battery Module Fault/New Batteries

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
igano_apc
Cadet
0 Likes
1
330

Symmetra LX SYAF16KRMT Battery Module Fault/New Batteries

This was originally posted on APC forums on 8/22/2013


HI,

We have a Symmetra LX system that will not come out of bypass mode because of a "Battery Module Fault". Originally the unit said it went into bypass mode because of a system overload, Failed MIM, Failed RIM, failed Power module, and failed Battery Module. The batteries in the system were just replaced with spares this morning and the fault is still present. the MIM, RIM, and Power Modules were also replaced today. I have also attempted to go into maintenance bypass mode and restart the unit. The system diags say that all the installed batteries are in "OK" status so why is the Power Module Fault still present? how do i get the unit out of bypass? any suggestions would be awesome. Oh! and before i'm asked below you will find the info from each battery (SN's Withheld).

Battery 1   Battery 2Battery 3Battery 4

FW REV: 10

SN: N/A

FW REV: 10

SN: N/A

FW REV: 10

SN: N/A

FW REV: 10

SN: N/A

Model: SYBT5

Model: SYBT5Model: SYBT5Model: SYBT5
MFG: 03/12MFG: 11/10MFG: 08/05MFG: 08/05

-0.00 1.97 864

4000 0 28 21

-00.0 2.16 864

4000 0 27 40

-00.1 2.11 864

4000 0 26 26

-0.00 1.98 864

4000 0 24 24

11FFFT

1.00 0705.7

0800.8 0000.0

11FFFT

1.00 0705.7

0800.8 0000.0

11FFFT

1.00 0704.8

0800.4 0000.0

11FFFT

1.00 0705.5

0800.5 0000.0


Accepted Solutions
Battman_apc
Commander
Commander
0 Likes
0
330

Re: Symmetra LX SYAF16KRMT Battery Module Fault/New Batteries

This was originally posted on APC forums on 8/23/2013


Was just noticing you appear to have a 50/50 mix of newer ( 2010/2012) and very old (2005) battery modules, which is not best practice and is not recommended by any UPS manufacturer. If the older cells have deteriorated and are showing higher impedance that may actually cause the system battery bus voltage to be lower than it should be.  If this were my system I would immediately pull battery 3 and 4 and see if that improves things....

See Answer In Context

1 Reply 1
Battman_apc
Commander
Commander
0 Likes
0
331

Re: Symmetra LX SYAF16KRMT Battery Module Fault/New Batteries

This was originally posted on APC forums on 8/23/2013


Was just noticing you appear to have a 50/50 mix of newer ( 2010/2012) and very old (2005) battery modules, which is not best practice and is not recommended by any UPS manufacturer. If the older cells have deteriorated and are showing higher impedance that may actually cause the system battery bus voltage to be lower than it should be.  If this were my system I would immediately pull battery 3 and 4 and see if that improves things....