Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84654members
354004posts

Smart-UPS and cold temps

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
lunadesign_apc
Crewman
Crewman
0 Likes
2
295

Smart-UPS and cold temps

This was originally posted on APC forums on 4/6/2010


I've got Verizon FiOS fiber optics in our building but their ONT (optical network terminal) is installed in an unheated garage. Their device comes with a weak battery backup unit that doesn't supply enough runtime. The garage generally stays above freezing but there have been a few occasions where it has dipped into the 20's for a few days.

I know the Smart-UPS units are rated for 32 - 104 °F but I'm curious if anyone has any experience running them at or slightly below the low end of that range. Do they shut off at 32 or is this 32 degree figure a conservative number where the performance of the unit degrades?


Accepted Solutions
shasuren_apc
Lieutenant
Lieutenant
0 Likes
0
295

Re: Smart-UPS and cold temps

This was originally posted on APC forums on 4/9/2010


You can use the UPS little below that temp range, but the battery and UPS life span may reduce.

See Answer In Context

2 Replies 2
Erasmus_apc
Sisko
Sisko
0 Likes
0
295

Re: Smart-UPS and cold temps

This was originally posted on APC forums on 4/6/2010


As far as APC's recommendations go, the "Usage Temperature" is the range at which the unit will function without risk to its internal electronics or the protected load. Additionally, this temperature range is meant to ensure an acceptable battery lifespan, as well as acceptable performance over that lifespan.

shasuren_apc
Lieutenant
Lieutenant
0 Likes
0
296

Re: Smart-UPS and cold temps

This was originally posted on APC forums on 4/9/2010


You can use the UPS little below that temp range, but the battery and UPS life span may reduce.