Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84416members
353604posts

Smart UPS 1500I -

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
BillP
Administrator Administrator
Administrator
0 Likes
1
179

Smart UPS 1500I -

This question was originally posted by Adam on APC forums on 2/6/2021


I had this unit for five years now. I always replaced batteries with genuine APC at least two times: not a single issue.

Recently, I have removed the UPS for scheduled maint, cleaned the ventilation holes and then put it back but without connecting any load. When I turned on the device, it performed a self-test which was not successful. The display showed a fault red light and the message: "fault state: output over volt". By attaching all the load back, and cycling the UPS power OFF-ON, the self-test was successfully passed. The load was 12% (120W).

If I attach something lower than 120W, the UPS won't pass the self-test neither is able to provide UPS protection to the outlets if the AC cable is removed (batteries fully charged).

Question #1:

Is there a Minimum load under which the UPS can't operate?

Question #2:

It is normal to get the "fault state: output over volt" without load?

I suspect a system malfunction because other UPS I have installed (different maker) are able to work and perform a self-test with no load attached. In this case, is there something I could do to verify the device?

Thank you very much,

Adam.


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
179

Re: Smart UPS 1500I -

This reply was originally posted by Adam on APC forums on 4/17/2021


After nearly two months, no answer!

Anyone?

 

Thank you,

AH

See Answer In Context

1 Reply 1
BillP
Administrator Administrator
Administrator
0 Likes
0
180

Re: Smart UPS 1500I -

This reply was originally posted by Adam on APC forums on 4/17/2021


After nearly two months, no answer!

Anyone?

 

Thank you,

AH