Welcome to the new Schneider Electric Community

It's your place to connect with experts and peers, get continuous support, and share knowledge.

Close
Important Announcement: WELCOME to the Schneider Electric Community! We have moved to a new address: community.se.com — bookmark it today and contact SchneiderCommunity.Support@se.com if you have any questions!
Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
82653members
350358posts

PowerChute Personal says the estimated battery time remaining is < 1 minute.

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
BillP
Administrator Administrator
Administrator
0 Likes
2
341

PowerChute Personal says the estimated battery time remaining is < 1 minute.

This question was originally posted by Aidan on APC forums on 1/22/2020


Hello, I seem to be having a problem with either my UPS or the PowerChute Personal Utility. It explains that I have < 1 minute of estimated battery time with 39% charge (as of right now) and an estimated 50w load out of 480. Anyways to make sure it wasn't the software just mucking up I reinstalled PowerChute as well as ran a self test and the results came out fine saying 'Passed' even though it tells me I have less then a minute if battery power left. I also see that the LED strip for "Replace Battery" is not lit up either, so the UPS itself is not detecting any problems, just PowerChute. Also another cause for concern is the fact that my remaining battery charge is 39% in the first place, because last time the UPS was transferred to the battery was a few weeks ago due to a power outage, none since. Although I do turn of my UPS every night after I have finished and turned off my PC so maybe that has something to do with it, but it still should not be this low. Just for reference the estimated remaining minutes is usually about 50 minutes at this wattage used. I appreciate any help.

Update 1: I decided to turn off my main PC and plug in a laptop with a 65w charger to the UPC to see if the UPS' battery would turn off in a minute or less, it didn't, I left it for about 5 minutes and it just made the beeps signifying that it was using battery power. It's either the the program or the USB cord I'm using since I just randomly found it around the house and decided to keep it plugged in since it worked, until now that might be.

Update 2: I have sourced another USB A to B cable and still the same results show. At this point I don't know what the issue could be.

Last update: I decided to unplug the UPS last night to see if it would turn on in the morning, it didn't which was concerning. So I plugged it back in turned it on and looked on the PowerChute software again, it now says it is at 99% charge (even though it didn't even turn on when it was unplugged) and also still says < 1 minute of battery time left. Self tests still passing and no red light on the "Replace Battery" strip.

Attachments
Tags (3)

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
341

Re: PowerChute Personal says the estimated battery time remaining is < 1 minute.

This reply was originally posted by Aidan on APC forums on 1/25/2020


I don't think you need to know my serial number but the model of my UPS is the BX950U-AZ.

See Answer In Context

2 Replies 2
BillP
Administrator Administrator
Administrator
0 Likes
0
341

Re: PowerChute Personal says the estimated battery time remaining is < 1 minute.

This reply was originally posted by Bill on APC forums on 1/24/2020


Hi,

What is the model of the Back-UPS and what is the serial number? Model and serial number information can be found in PowerChute under the technical data tab. 

BillP
Administrator Administrator
Administrator
0 Likes
0
342

Re: PowerChute Personal says the estimated battery time remaining is < 1 minute.

This reply was originally posted by Aidan on APC forums on 1/25/2020


I don't think you need to know my serial number but the model of my UPS is the BX950U-AZ.