Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84591members
353858posts

PowerChute Network Shutdown on OS X 10.6.8 Server -- SOLVED

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
BillP
Administrator Administrator
Administrator
0 Likes
3
299

PowerChute Network Shutdown on OS X 10.6.8 Server -- SOLVED

This question was originally posted by Matthew on APC forums on 2/11/2013


I have an APC SmartUPS RT 3000. I have the Network Management Card successfully installed and operating. I am attempting to install "PowerChute Network Shutdown v3.0.1" on my OS X 10.6.8 Server. I am unsuccessful thus far. I get to this screen (see below) and then the installer dies. I cannot connect to PCNS via a browser. By all accounts I do not see the necessary files. I do not see any files in /Library/StartupItems/comapcpcns. According to the manual, I can manually start the service by sudo /Library/StartupItems/comapcpcns/comapcpcns start. Kinda hard to do when the file doesn't exist.

TIA.

-Matt

Message was edited by: mncrnich

Attachments

Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
299

Re: PowerChute Network Shutdown on OS X 10.6.8 Server

This reply was originally posted by Angela on APC forums on 2/12/2013


I have a few questions:

• Are you installing this remotely in any way or physically with the server?
• Verify the path that PCNS is being installed to
• Provide the pcnsinst.log which would be in the folder wherever you downloaded PCNS to and launched it from (where ever install.cmd is)
• Run the uninstaller and report back if it completes without error

See Answer In Context

3 Replies 3
BillP
Administrator Administrator
Administrator
0 Likes
0
299

Re: PowerChute Network Shutdown on OS X 10.6.8 Server

This reply was originally posted by Matthew on APC forums on 2/13/2013


mncrnich wrote:
i picKed a winna wrote:
• Provide the pcnsinst.log which would be in the folder wherever you downloaded PCNS to and launched it from (where ever install.cmd is)
I looked over this log file. I saw a permission problem. I then uninstalled and attempted to re-install as "root". Well sure enough, that did it. Installation was successful as root user. PCNS is running.

I wish the documents would mention "root" user needs to perform the installation.

I hope this helps someone else out in the future.

Best,

Matt

BillP
Administrator Administrator
Administrator
0 Likes
0
299

Re: PowerChute Network Shutdown on OS X 10.6.8 Server

This reply was originally posted by Angela on APC forums on 2/13/2013


we were just looking at that as well! i was going to ask you what the permissions of that folder was.

anyway, I will tell the PowerChute folks so we can update applicable documents ASAP.

thanks for following up.

BillP
Administrator Administrator
Administrator
0 Likes
0
300

Re: PowerChute Network Shutdown on OS X 10.6.8 Server

This reply was originally posted by Angela on APC forums on 2/12/2013


I have a few questions:

• Are you installing this remotely in any way or physically with the server?
• Verify the path that PCNS is being installed to
• Provide the pcnsinst.log which would be in the folder wherever you downloaded PCNS to and launched it from (where ever install.cmd is)
• Run the uninstaller and report back if it completes without error