Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84865members
354354posts

Internal hardware fault reported with NMC3 card 2.2.0.1 firmware

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Phil34_apc
Crewman
Crewman
0 Likes
3
529

Internal hardware fault reported with NMC3 card 2.2.0.1 firmware

Hello,

 

I have a new APC SRT10KRMXLI with a AP9640 NMC3 Card.

 

The factory version was : v1.3.3.1

 

apc>about

E000: Success

Hardware Factory

---------------

Model Number:           0N-1557

Serial Number:          5A2205T54882

Hardware Revision:      3

Manufacture Date:       02/05/2022

MAC Address:            28 29 86 66 97 5D

Management Uptime:      0 Days 20 Hours 48 Minutes

 

Application Module

---------------

Name:                   su

Version:                v1.3.3.1

Date:                   Jul 24 2020

Time:                   19:53:52

 

APC OS(AOS)

---------------

Name:                   aos

Version:                v1.3.3.1

Date:                   Jul 24 2020

Time:                   19:53:52

 

APC Boot Monitor

---------------

Name:                   boot

Version:                v1.1.0.2

Date:                   Mar 29 2019

Time:                   12:27:11

 

I had no issues with this version since the card had been configured.

 

I downloaded the last firmware : apc_hw21_su_2-2-0-1.exe.

The update was a success, but now the NMC card reports regularly an internal issue :

 

Jun 15 16:25:15 UPS: In bypass in response to an internal hardware fault. 0x011B
Jun 15 16:25:16 UPS: Return from bypass, internal hardware fault no longer present. 0x01B2
Jun 15 16:37:35 UPS: In bypass in response to an internal hardware fault. 0x011B
Jun 15 16:37:35 UPS: Return from bypass, internal hardware fault no longer present. 0x01B2
Jun 15 17:20:34 UPS: In bypass in response to an internal hardware fault. 0x011B
Jun 15 17:20:35 UPS: Return from bypass, internal hardware fault no longer present. 0x01B2

 

Show the new version :

 

apc>about
E000: Success
Hardware Factory
---------------
Model Number: 0N-1557
Serial Number: 5A2205T54882
Hardware Revision: 3
Manufacture Date: 02/05/2022
MAC Address: 28 29 86 66 97 5D
Management Uptime: 0 Days 1 Hour 56 Minutes

Application Module
---------------
Name: su
Version: v2.2.0.1
Date: Mar 24 2022
Time: 19:06:03

APC OS(AOS)
---------------
Name: aos
Version: v2.2.0.1
Date: Mar 24 2022
Time: 19:06:03

APC Boot Monitor
---------------
Name: boot
Version: v1.4.2.1
Date: Mar 21 2022
Time: 11:45:57

 

I reboot the NMC card, cut off the main power, the issue remains.

 

An idea of the problem ?

The UPS is not yet powering the servers, but I would like a solution of these messages.

 

Thank you

Tags (1)
3 Replies 3
Phil34_apc
Crewman
Crewman
0 Likes
2
526

Re: Internal hardware fault reported with NMC3 card 2.2.0.1 firmware

Sorry, my card is an AP9641

Tags (1)
BillP
Administrator Administrator
Administrator
0 Likes
1
500

Re: Internal hardware fault reported with NMC3 card 2.2.0.1 firmware

@Phil34_apc 

 

This is a know issue with the firmware. We had published a FAQ but it appears to have been moved. Below is a copy

 

Issue:
After upgrading to SU v2.2.0.1, event log shows multiple bypass events, even on UPS systems that do not support bypass

Product Line:
SU application module for Network Management Card 3 devices

Cause:
This is caused by an NMC firmware bug

Resolution:
This issue will be addressed in a future firmware release. There are a few current options for remediation:

  • Downgrade NMC firmware to SU v2.0  https://schneider-electric.box.com/s/j0fm974afgh8t1sh7czzayk7huyrjjug 
  • On UPS systems with bypass, add a delay on the event for 2 seconds or greater. The events triggered by this bug are immediately cleared, so this will prevent email spam from erroneous bypass events
  • On UPS systems without bypass, these events can be disabled completely

After flashing a card with firmware that resolves this issue, it's recommended to reset any event configurations back to what they were. 

Tags (1)
Phil34_apc
Crewman
Crewman
0 Likes
0
470

Re: Internal hardware fault reported with NMC3 card 2.2.0.1 firmware

@BillPThanks a lot for your answer !

 

I'm sure it's not a hardware defect.

i will be waiting for the new firmware, and I set the email delay to 5 seconds (it's the minimum value). That prevents sending emails.

 

 

Have a nice day

Tags (1)