Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84817members
354269posts

Installation question with spare battery pack on a SUA3000XL

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
scrowe_apc
Crewman
Crewman
0 Likes
4
209

Installation question with spare battery pack on a SUA3000XL

This was originally posted on APC forums on 11/17/2008


We currently have an SUA3000XL in the office, running our NAS, a few monitoring computers, and other devices. The boss has decided to splurge and buy 2 Battery packs (XL48V) and wants me to plug them into the main UPS.

We don't run Powerchute on any system attached to the UPS, since we don't actually have any Windows machines nearby. Is it going to be safe to connect the battery packs up to the main UPS, or do I need to have it hooked to a PC first to tell it it's going to have 2 Battery packs attached?

Thanks everyone.


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
209

Re: Installation question with spare battery pack on a SUA3000XL

This reply was originally posted by Angela on APC forums on 11/18/2008


you can physically add/plug in the batteries safely and the UPS will use those batteries. the only thing it wont do is calculate the runtime correctly and also as you kind of mentioned, the powerchute software would need that to shut items down accordingly. it will just work fine in your situation - no need to tell the UPS it has extra battery packs.

See Answer In Context

4 Replies 4
scrowe_apc
Crewman
Crewman
0 Likes
0
209

Re: Installation question with spare battery pack on a SUA3000XL

This was originally posted on APC forums on 11/18/2008


Thanks so much for your help!

BillP
Administrator Administrator
Administrator
0 Likes
0
210

Re: Installation question with spare battery pack on a SUA3000XL

This reply was originally posted by Angela on APC forums on 11/18/2008


you can physically add/plug in the batteries safely and the UPS will use those batteries. the only thing it wont do is calculate the runtime correctly and also as you kind of mentioned, the powerchute software would need that to shut items down accordingly. it will just work fine in your situation - no need to tell the UPS it has extra battery packs.

scrowe_apc
Crewman
Crewman
0 Likes
0
209

Re: Installation question with spare battery pack on a SUA3000XL

This was originally posted on APC forums on 11/18/2008


Thanks for your prompt reply 🙂

Before I go fiddling around: do I need to have the UPS off when I plug them in? And is there an order I should plug then in at all?

eg: I have:

UPS BAT1 BAT2
\---------| \---------|
Do I plug BAT2 into BAT1, then BAT1 into UPS, or BAT1 into UPS, then BAT2 into BAT1?

BillP
Administrator Administrator
Administrator
0 Likes
0
209

Re: Installation question with spare battery pack on a SUA3000XL

This reply was originally posted by Angela on APC forums on 11/18/2008


these are hot swappable so you can go ahead and plug them in hot. just be careful not to hit any other power plugs, etc 😛

You'd plug the Bat 1 into the back of the UPS (which the port for the external battery may have a cover on it right now, I forget with this model off the top of my head - so you may need to remove that), then plug Bat 2 into the back of Bat 1 and you're all set!

it doesnt matter what order you do this - whatever is easier. you could plug Bat 2 into Bat 1 then connect Bat 1 into the UPS or just do it individually.