Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84420members
353605posts

How can I use an SSH private/public keypair with the AP9630 management card?

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
andyt22_apc
Crewman
Crewman
0 Likes
3
205

How can I use an SSH private/public keypair with the AP9630 management card?

This was originally posted on APC forums on 3/18/2013


I want to be able to log into a AP9630 UPS management card using a SSH private/public keypair instead of having to type in a password every time - is this possible? I have tried to scp an SSH public key from a Linux PC into the /ssh folder on a AP9630 but I keep getting 'connection lost' messages even though I can log into the system via SSH.

The reason I want to do this is if a server room temperature exceeds a certain threshold, a script running on a thermal monitoring PC will log into a UPS via SSH and shut it down, removing power from the servers, etc that the UPS feeds power to. If this is not possible via SSH, is there any other way I can get the UPS to power off unattended?

Thanks, Andy  


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
205

Re: How can I use an SSH private/public keypair with the AP9630 management card?

This reply was originally posted by Angela on APC forums on 3/18/2013


I am not sure if this is an option either but with an AP9631 network management card, it has an ambient temperature probe that comes with it that could be used to gracefully shutdown any PowerChute Network shutdown clients when there is a temperature violation (meaning any violation - too hot, too cold) and then the UPS itself after that's done. I am not sure if that would work for you if you replaced the AP9630's. scripting may be just as easy for you also and save money.

See Answer In Context

3 Replies 3
BillP
Administrator Administrator
Administrator
0 Likes
0
205

Re: How can I use an SSH private/public keypair with the AP9630 management card?

This reply was originally posted by Angela on APC forums on 3/18/2013


i don't think so - you can use the keys in general but i don't believe there is a way to get around the password requirement for authentication. might I suggest SNMP instead and doing a SET? you could do some type of CLI SNMP such as snmpset maybe.

andyt22_apc
Crewman
Crewman
0 Likes
0
205

Re: How can I use an SSH private/public keypair with the AP9630 management card?

This was originally posted on APC forums on 3/18/2013


Thanks, I have never used snmp before so I will look into this.

The problem I have is if there is a power failure, even a brief one, the cooling systems will stop and will not restart when power returns as they have to be manually restarted. Meanwhile, the entire server room is on multiple UPS units and will continue creating heat so I'd rather shut down everything by removing almost all power, as some servers will shut down but not power off.

Andy

BillP
Administrator Administrator
Administrator
0 Likes
0
206

Re: How can I use an SSH private/public keypair with the AP9630 management card?

This reply was originally posted by Angela on APC forums on 3/18/2013


I am not sure if this is an option either but with an AP9631 network management card, it has an ambient temperature probe that comes with it that could be used to gracefully shutdown any PowerChute Network shutdown clients when there is a temperature violation (meaning any violation - too hot, too cold) and then the UPS itself after that's done. I am not sure if that would work for you if you replaced the AP9630's. scripting may be just as easy for you also and save money.