Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84494members
353715posts

Environment probe SNMP

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
vobelic_apc
Crewman
Crewman
0 Likes
3
227

Environment probe SNMP

This was originally posted on APC forums on 10/10/2016


Hello,

I own an older UPS surt3000xl with AP9619 and a temperature probe.

From what I googled, OID .1.3.6.1.4.1.318.1.1.10.2.3.2.1.4.1 should be the one for temperature output.

Thing is, it's integer value, so no decimals are available.

On the other hand, on the webUI i'm normally seeing decimal values for the environment probe temperature output.

Is this a limitation or?

UPS FW: 450.17.W

AP9619    
sumx v3.7.2
aos  v3.7.3

Thanks in advance.


Accepted Solutions
BillP
Administrator Administrator
Administrator
0 Likes
0
227

Re: Environment probe SNMP

This reply was originally posted by Shanon on APC forums on 10/17/2016


Hello Vladimir,

Voidstar is correct, there is no high precision OID for the temperature probe. 

See Answer In Context

3 Replies 3
voidstar_apc
Janeway
Janeway
0 Likes
0
227

Re: Environment probe SNMP

This was originally posted on APC forums on 10/10/2016


SNMP only supports integers. As a workaround, some OIDs have a corresponding high precision OID that reports in tenths or hundredths. I don't see any such OIDs for the temperature probe.

To explore all the OIDs available, I recommend downloading the PowerNet MIB (from here listed as "Firmware Upgrade - MIB"). Use it with a free tool GetIF (available here) and walk the target system to see everything it supports.

vobelic_apc
Crewman
Crewman
0 Likes
0
227

Re: Environment probe SNMP

This was originally posted on APC forums on 10/15/2016


Hi,

I've expressed myself wrongly here. I am aware SNMP outputs only integers.

By integer value in output of .1.3.6.1.4.1.318.1.1.10.2.3.2.1.4.1 I meant it isn't high precision.

So far I used the high precision UPS internal battery temperature OID .1.3.6.1.4.1.318.1.1.1.2.3.2.0 but I can't seem to find the high precision version for environment probes.

I assume a high precision OID for this should be available since I see probe temperature readings in the WebUI in precision in tenths.

Can someone confirm there's no high precision OID for probe temperature values in AP9619 ?

BillP
Administrator Administrator
Administrator
0 Likes
0
228

Re: Environment probe SNMP

This reply was originally posted by Shanon on APC forums on 10/17/2016


Hello Vladimir,

Voidstar is correct, there is no high precision OID for the temperature probe.