Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84342members
353519posts

Does Masterswitch Plus AP9225EXP + AP9606 = AP9225 w/APC installed AP9606?

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
dansurplusman_apc
Crewman
Crewman
0 Likes
5
254

Does Masterswitch Plus AP9225EXP + AP9606 = AP9225 w/APC installed AP9606?

This was originally posted on APC forums on 7/28/2007


I picked up two MasterSwitch Plus "expansion cabinets", Model AP9225EXP, each of which had an AP9606 SNMP card installed (presumably by a prior owner). As I understand it, the 9225EXP does not come with the AP9606 pre-installed, as it is designed to "slave" off a 9225 with the card factory installed by APC. The question I have is, if one does install an AP9606 in an AP9225EXP, does one end up with a unit with 100% of the functionality of a factory-created AP9225 with the factory installed AP9606? Also, aside from Masterswitch-to-UPS cabling, does one need a specially wired console cable to communicate with a MasterSwitch for configuration purposes (and if so, which APC cables will do the job, in addition to any actually specified in the user guide), or will a standard straight-through serial cable, or a null modem cable, do the job? Thanks. -- Dan


Accepted Solutions
seoerming1_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
254

Jeremy Scott

This was originally posted on APC forums on 3/23/2011


The progress on the electrical lines at the Fukushima Jeremy Scott Dai-ichi nuclear power plant was a welcome and Jeremy Scott Shoes significant advance Tuesday after days of setbacks. With the power lines connected, officials Jeremy Scott Shop hope to start up the overheated plant's crucial cooling system that was knocked out during the March 11 earthquake Jeremy Scott Adidas and tsunami that devastated Japan's northeast coast. Tokyo Electric Power Co. warned that workers still need to check all equipment Jeremy Scott Wings for damage first before switching the cooling system on to all the reactor units — a process that Jeremy Scott JS Wings ould take days or even weeks. Late Tuesday night, Tokyo Electric said lights went on in the central control room of Unit 3, but that doesn't mean power had been restored to the cooling system.

See Answer In Context

5 Replies 5
dirtfoot_apc
Lt. Commander
Lt. Commander
0 Likes
0
254

Re: Does Masterswitch Plus AP9225EXP + AP9606 = AP9225 w/APC installed AP9606?

This was originally posted on APC forums on 7/30/2007


Yeah, you should be able to put in your own AP9606 if you've got one, and use it in the EXP unit. It will have the same functionality as the AP9225. Just make sure you put the correct firmware on your AP9606 because I'm guessing it didn't originally come out of a MasterSwitch.

ftp://ftp.apcc.com/apc/public/hardware/mswitch/firmware/msp/v200/



You can also install an AP9617 management card in the MasterSwitch, and use this firmware:
http://www.apcc.com/tools/download/software_comp.cfm?sw_sku=SFMSP262

Grenade_apc
Lieutenant
Lieutenant
0 Likes
0
254

Re: Does Masterswitch Plus AP9225EXP + AP9606 = AP9225 w/APC installed AP9606?

This was originally posted on APC forums on 10/30/2007


These two cards have built in Web Cards and they do not support upgrading to a newer network management card.

BillP
Administrator Administrator
Administrator
0 Likes
0
254

Re: Does Masterswitch Plus AP9225EXP + AP9606 = AP9225 w/APC installed AP9606?

This reply was originally posted by Jim on APC forums on 10/30/2007


Does the MasterSwitch VMcontroller ( AP9224 or AP9221nx166 ) support upgrading to the newer Web/SNMP card too?

KVM4Life_apc
Lieutenant
Lieutenant
0 Likes
0
254

Re: Does Masterswitch Plus AP9225EXP + AP9606 = AP9225 w/APC installed AP9606?

This was originally posted on APC forums on 11/12/2007


Hello,

The new Switched Rack PDUs use the newer Network Managment Card (AP9617) technology.

The link below is a NEMA 5-15 input/NEMA 5-15 output.

http://www.apc.com/resource/include/techspec_index.cfm?base_sku=AP7931

seoerming1_apc
Lieutenant JG
Lieutenant JG
0 Likes
0
255

Jeremy Scott

This was originally posted on APC forums on 3/23/2011


The progress on the electrical lines at the Fukushima Jeremy Scott Dai-ichi nuclear power plant was a welcome and Jeremy Scott Shoes significant advance Tuesday after days of setbacks. With the power lines connected, officials Jeremy Scott Shop hope to start up the overheated plant's crucial cooling system that was knocked out during the March 11 earthquake Jeremy Scott Adidas and tsunami that devastated Japan's northeast coast. Tokyo Electric Power Co. warned that workers still need to check all equipment Jeremy Scott Wings for damage first before switching the cooling system on to all the reactor units — a process that Jeremy Scott JS Wings ould take days or even weeks. Late Tuesday night, Tokyo Electric said lights went on in the central control room of Unit 3, but that doesn't mean power had been restored to the cooling system.