Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84849members
354308posts

Cannot add host to Host Protection UPS (PowerChute)

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

hmi
Cadet
0 Likes
3
167

Cannot add host to Host Protection UPS (PowerChute)

Dear community,

 

I can see all hosts under PCNS -> Host Protection on the left side under my Data Center but I can not move it to the right side to match with the correct UPS.

 

I attached a screenshot - the hosts on the left side are greyed out and I can not drag and drop them.

 

We have 2 UPS and 3 Hosts

The main host (running PCNS and vCenter) is matched with the correct UPS, but I would like to match the the other hosts with the second UPS shown.

 

Am I missing something?

Any help would be greatly appreciated.

 

PCNS 4.4.3 and vCenter/ESXI 7

Attachments
Tags (1)
3 Replies 3
BillP
Administrator Administrator
Administrator
0 Likes
2
145

Re: Cannot add host to Host Protection UPS (PowerChute)

@hmi 

 

Are you seeing a Red X when you drag the host to the UPS? If so that indicates you are attempting to add the host to the UPS, and you need to add the host to an outlet group. 

 

If the hosts are grayed out that indicates the host has been added to a UPS or outlet group. You will find the lists of assigned host in the pcnsconfig.ini file.

 

Examples

[advanced_ups_setup_0]
setup_name = SMT1500

hostlist = 192.168.0.141&1

 

[advanced_ups_setup_1]
setup_name = SMTL1000

hostlist = 192.168.0.176&1|192.168.0.144&1|192.168.0.128&1

 

 

Attachments
Tags (1)
hmi
Cadet
0 Likes
1
134

Re: Cannot add host to Host Protection UPS (PowerChute)

Thank you for the quick reply @BillP.

 

There is no red X, it's grayed out and there is just that forbidden icon (black crossed circle).

 

I checked the ini and I can see the following

 

hostlist = host1.domain.com|host2.domain.com

 

I noticed you have the '&1' in there. Is that mandatory?

I didn't edit the config manually before, so that is what the wizard put in there.

Tags (1)
BillP
Administrator Administrator
Administrator
0 Likes
0
85

Re: Cannot add host to Host Protection UPS (PowerChute)

@hmi 

 

Try clearing the browser data, and then log in to the PowerChute UI. If the UI still does not display the hosts in the list, log out of the UI. Then log in to the PowerChute VM and stop the PowerChute service; the command is systemctl stop PowerChute. Next, edit the pcnsconfig.ini and remove the hosts from the list hostlist = host1.domain.com|host2.domain.com. Next, restart the PowerChute service (systemctl start PowerChute) and log in to the PowerChute UI. You should see the hosts available to add to the list.

 

To answer the question about the &number, that will be inserted if the associated UPS has switched outlet groups. In my example, I had each host associated with a UPS with outlet groups, and each was associated with group 1. 

Tags (1)