Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84695members
354073posts

AP9641 reboots every 10 minutes

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
MikeH
Crewman
Crewman
0 Likes
4
647

AP9641 reboots every 10 minutes

Have been going around for a while trying to get this management card to stop doing the watchdog timer reboot.  I've set it to use static IPs as well as DHCP and can't seem to find any way to make it stop.  How do I resolve this, or disable the watchdog timer? Firmware has been updated to v2.2.0.1.

Tags (1)

Accepted Solutions
Matt-B
Lieutenant JG Lieutenant JG
Lieutenant JG

Re: AP9641 reboots every 10 minutes

Hello,

 

We've seen restarts like this on cards that were at one time running firmware version v1.6.1.1 or earlier. To fix it, after upgrading to v2.2.0.1 you can download the config.ini file, then format the NMC using one of two methods:

 

  • Boot loader: Connect to the NMC3 via the Console Port.  Restart the NMC3.  Within 4-5 seconds of restart, press the <enter> key to interrupt the boot loader.  From the BM> prompt, type “format”.  Once the format is complete, type “reset”, the NMC3 should restart and boot normally.

 

  • Reset button: Press and hold the reset button located at the front of the NMC3, for at least 20 seconds, or until the Status LED begins to blink orange.  Allow the NMC3 to restart.

 

After the format, you can upload the saved config.ini file to preserve the settings that the format erased. For simplicity sake, I'd recommend using the reset button to format. 

See Answer In Context

Tags (1)
4 Replies 4
Matt-B
Lieutenant JG Lieutenant JG
Lieutenant JG

Re: AP9641 reboots every 10 minutes

Hello,

 

We've seen restarts like this on cards that were at one time running firmware version v1.6.1.1 or earlier. To fix it, after upgrading to v2.2.0.1 you can download the config.ini file, then format the NMC using one of two methods:

 

  • Boot loader: Connect to the NMC3 via the Console Port.  Restart the NMC3.  Within 4-5 seconds of restart, press the <enter> key to interrupt the boot loader.  From the BM> prompt, type “format”.  Once the format is complete, type “reset”, the NMC3 should restart and boot normally.

 

  • Reset button: Press and hold the reset button located at the front of the NMC3, for at least 20 seconds, or until the Status LED begins to blink orange.  Allow the NMC3 to restart.

 

After the format, you can upload the saved config.ini file to preserve the settings that the format erased. For simplicity sake, I'd recommend using the reset button to format. 

Tags (1)
MikeH
Crewman
Crewman
0 Likes
2
629

Re: AP9641 reboots every 10 minutes

Thanks that did the trick! Actually this UPS is on a remote site so didn't have physical access.  I was able to accomplish the same thing though by going in via SSH and doing a format command then a reboot.

Tags (1)
Shaun
Lt. Commander Lt. Commander
Lt. Commander

Re: AP9641 reboots every 10 minutes

Hi @MikeH,

 

The easier option was left out intentionally - we've noticed that if the affected file is deleted, or the card is formatted online (the method you've used while the card is running) - sometimes the issue returns, sometimes it doesn't.

 

Just something to keep in mind if the issue returns, or for anyone else searching this topic.  If the shortcut works - great.  If it comes back, it may need a heavier touch.

 

Thanks,

  Shaun

Tags (1)
J-E-1984
Ensign
Ensign
0 Likes
0
143

Re: AP9641 reboots every 10 minutes

Seems we're in "Heavier Touch" areas as we have the same issue... 

Tags (1)