Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84589members
353854posts

AP7175 FW v3.7.3 AOS v3.7.3

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
knowlesy_apc
Ensign
Ensign
0 Likes
3
243

AP7175 FW v3.7.3 AOS v3.7.3

This was originally posted on APC forums on 6/4/2015


Hi I have two AP7175, I am trying to update them to the latest versions http://www.apc.com/products/resource/include/techspec_index.cfm?base_sku=AP7175&tab=software howeverwhen trying either of the updates for FW or AOS its stating that it is 2 revisions behind 

Log from upgrade

"Before Upgrading the NMC the AOS is: ÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌÌp(È
* Detected early version, two AOS upgrades required"

Where do I find older versions to update  ?

cheers

 


Accepted Solutions
Terry_Kennedy_apc
Commander
Commander
0 Likes
0
243

Re: AP7175 FW v3.7.3 AOS v3.7.3

This was originally posted on APC forums on 6/4/2015


It is odd that the utility is behaving the way it is, then. Is it possible that you have a firewall or network issue?

If you are sure that there is no problem communicating with the device, you could manually FTP the update files to it. First, FTP the AOS file (the newer of the 2 with aos in the name in the directory you specified when installing the update utility). Once you log out, the device should reboot (could take up to 2 minutes). Then FTP the application to it (in this case, the file with rpdu in the name). Once you log out, the device should reboot again, and at that point you should be able to log in (wait a minute or so for the reboot to complete) and you should see the new versions on the first page.

Once you're running the new version, you may want to configure a time server on the unit (in the picture you posted, it thinks it is 2005) so you can easily compare event timestamps with real-world times.

See Answer In Context

3 Replies 3
Terry_Kennedy_apc
Commander
Commander
0 Likes
0
243

Re: AP7175 FW v3.7.3 AOS v3.7.3

This was originally posted on APC forums on 6/4/2015


Normally the upgrade utility will detect and handle old AOS versions automatically. The download includes AOS 2.0.2 as an intermediate update if the existing firmware is older than that.

However, it looks like the utility is reporting garbage for the AOS version installed on the device. If you telnet to the device, what do you see for the currently installed version (both AOS and application)?

knowlesy_apc
Ensign
Ensign
0 Likes
0
243

Re: AP7175 FW v3.7.3 AOS v3.7.3

This was originally posted on APC forums on 6/4/2015


Hi it has 3.7.0 for both see attached 

Attachments
Terry_Kennedy_apc
Commander
Commander
0 Likes
0
244

Re: AP7175 FW v3.7.3 AOS v3.7.3

This was originally posted on APC forums on 6/4/2015


It is odd that the utility is behaving the way it is, then. Is it possible that you have a firewall or network issue?

If you are sure that there is no problem communicating with the device, you could manually FTP the update files to it. First, FTP the AOS file (the newer of the 2 with aos in the name in the directory you specified when installing the update utility). Once you log out, the device should reboot (could take up to 2 minutes). Then FTP the application to it (in this case, the file with rpdu in the name). Once you log out, the device should reboot again, and at that point you should be able to log in (wait a minute or so for the reboot to complete) and you should see the new versions on the first page.

Once you're running the new version, you may want to configure a time server on the unit (in the picture you posted, it thinks it is 2005) so you can easily compare event timestamps with real-world times.