Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84331members
353498posts

9619 output realy

APC UPS Data Center & Enterprise Solutions Forum

Schneider Electric support forum for our Data Center and Business Power UPS, UPS Accessories, Software, Services, and associated commercial products designed to share knowledge, installation, and configuration.

Solved
cometmth_apc
Crewman
Crewman
0 Likes
10
827

9619 output realy

This was originally posted on APC forums on 9/25/2008


I would like to use the output realy of the 9619 management card to control an external device based on alarm conditions from the UPS. I can see and understand the options in the software for controlling this, but my question is on the physical side. It would appear that you need some sort of bracket/cable thing to connect to the pins on the back of the 9619. Also, I'm not sure which of the pins to use for the output relay. has anyone actually set up the output relay or input contacts on any of the management cards? I'm looking for any help I can get.

[http://www.apc.com/products/moreimages.cfm?partnum=AP9619&aPos=2|http://www.apc.com/products/moreimages.cfm?partnum=AP9619&aPos=2]

Thanks


Accepted Solutions
cometmth_apc
Crewman
Crewman
0 Likes
0
827

Re: 9619 output realy

This was originally posted on APC forums on 10/1/2008


So I just pull the blue part off, attach wires to it, and snap it back on?

See Answer In Context

10 Replies 10
voidstar_apc
Janeway
Janeway
0 Likes
0
827

Re: 9619 output realy

This was originally posted on APC forums on 10/4/2008


Yes.

vcwaterboy_apc
Cadet
0 Likes
0
827

Re: 9619 output realy

This was originally posted on APC forums on 8/17/2009


Does any of you know the maximum voltage that can run through those relay output?
Thanks.

Techie_apc
Admiral
Admiral
0 Likes
0
827

Re: 9619 output realy

This was originally posted on APC forums on 8/17/2009


Thang,

The Current capacity of relay contacts: 1 A @ 30 V AC/DC (for AP9618 and AP9619 only)
+12 VDC output: 25 mA maximum current (for AP9618 and AP9619
only)

More information can be found on the page # 21 in the below link:
http://www.apcmedia.com/salestools/ASTE-6Z5QDZ_R0_EN.pdf

vcwaterboy_apc
Cadet
0 Likes
0
827

Re: 9619 output realy

This was originally posted on APC forums on 8/17/2009


Thank you, but can you be a little more specific? Since I'm not really an electrician.
I'm confusing between the 1A at 30 V AC/DC and the 12 VDC at 25 mA.
Can I use 24 vDC?
Thanks again

Techie_apc
Admiral
Admiral
0 Likes
0
827

Re: 9619 output realy

This was originally posted on APC forums on 8/17/2009


Thang,

Here is what I got for you:

You can pass up to 30 V through it. However, you need to make sure that your equipment can handle it on the other end and your resistance is set up correctly.

So answer to your question is that you can use 24 V and the card can provide up to 12 V if you need it to. However, I recommend you to have someone who has an experience to wire this as to not damage the card or equipment.

Message was edited by: Techie

Cap1_apc
Lt. Commander
Lt. Commander
0 Likes
0
827

Re: 9619 output realy

This was originally posted on APC forums on 10/16/2008


This was designed like this for a reason - it's a lot easier to wire the blue terminal piece and pop it back into the card. The alternative would be trying to wire the card directly while installed in the UPS, which could lead to you accidentally yanking the card out or becoming very frustrated while laying on the floor with a mini screwdriver 😉

BillP
Administrator Administrator
Administrator
0 Likes
0
827

Re: 9619 output realy

This reply was originally posted by Yuri on APC forums on 12/6/2011


Please help me to connect to relay contacts of 9619 card...
I don't know meaning of 4 contacts at left group (output relay)
Which of them normally connected or disconnected?
I wont to build light or sound sign if room overheat...

thanks, Yuri

BillP
Administrator Administrator
Administrator
0 Likes
0
826

Re: 9619 output realy

This reply was originally posted by Angela on APC forums on 12/6/2011


you first need to decide if your relay is going to be normally open or normally closed. for the output, once you device, then wire up to NO or NC and COM. i dont think you should need to use the other connections on the output.

EZ_Button_apc
Commander
Commander
0 Likes
0
826

Re: 9619 output realy

This was originally posted on APC forums on 9/25/2008


The card comes with an attachment piece that sticks out of the unit. You insert the wire and tighten a screw to secure the contact. There is a picture of it below.

http://www.apc.com/resource/include/techspec_index.cfm?base_sku=AP9619

cometmth_apc
Crewman
Crewman
0 Likes
0
828

Re: 9619 output realy

This was originally posted on APC forums on 10/1/2008


So I just pull the blue part off, attach wires to it, and snap it back on?