Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Schneider Electric Community
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
  • About Kwon
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Kwon
Kwon
Contributor
‎2026-10-11
6
Posts
0
Likes Received
0
Likes Given
0
Solutions

Community Badges

Open Hailing Frequencies
Resistance is Futile
Mind Meld
There's coffee in that nebula.
+1
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
Kwon
Kwon

Can the A9MEM1560 product be used for single-phase L-L 208V

I have an additional question.In the 208V 3-phase, 3-wire system mentioned above, if UL certification is not required,can the A9MEM1560 be used for P...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
142 0 2

2026-09-28 02:13 AM

Kwon
Kwon

Can the A9MEM1575 product be used for single-phase L-L 208V or 3-phase...

We are planning to select a Powertag product with UL certification for a power system like the one shown in the photo below. Can the A9MEM1575 model ...
EcoStruxure Power & Grid icon_circle Metering & Power Quality
287 0 5

2026-09-20 06:51 PM

Activity Feed
  • Posted RE: Can the A9MEM1560 product be used for single-phase L-L 208V on Metering & Power Quality. ‎2026-09-28 09:43 PM
  • Posted Can the A9MEM1560 product be used for single-phase L-L 208V on Metering & Power Quality. ‎2026-09-28 02:13 AM
  • Tagged Can the A9MEM1560 product be used for single-phase L-L 208V on Metering & Power Quality. ‎2026-09-28 02:13 AM
  • Posted Re: Can the A9MEM1575 product be used for single-phase L-L 208V or 3-phase 208V applications? on Metering & Power Quality. ‎2026-09-22 07:34 PM
  • Posted Re: Can the A9MEM1575 product be used for single-phase L-L 208V or 3-phase 208V applications? on Metering & Power Quality. ‎2026-09-22 05:44 PM
  • Posted Re: Can the A9MEM1575 product be used for single-phase L-L 208V or 3-phase 208V applications? on Metering & Power Quality. ‎2026-09-22 05:43 PM
  • Posted Can the A9MEM1575 product be used for single-phase L-L 208V or 3-phase 208V applications? on Metering & Power Quality. ‎2026-09-20 06:51 PM
  • Tagged Can the A9MEM1575 product be used for single-phase L-L 208V or 3-phase 208V applications? on Metering & Power Quality. ‎2026-09-20 06:51 PM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.