Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Schneider Electric Community
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
  • About Kasper.Vestrup
Options
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Kasper.Vestrup
Kasper.Vestrup
Explorer
‎2026-09-08
144
Posts
2
Likes Received
0
Likes Given
0
Solutions

Community Badges

Resistance is Futile - L7
Resistance is Futile - L6
Resistance is Futile - L5
Resistance is Futile - L4
+7
View All
  • Latest Posts
  • Likes Given
  • Latest Contributions
  • Activity Feed
Kasper.Vestrup
Kasper.Vestrup Explorer

Experior & Remote Viewer – OpenID Connect (OIDC) Login Guide

OverviewThis document explains how to enable OpenID Connect (OIDC) authentication for Experior and the Experior Remote Viewer. Once configured, users ...
Knowledge Center icon_circle Digital Twin
353 0 0

2026-05-26 02:06 AM

Kasper.Vestrup
Kasper.Vestrup Explorer

Navigating Remote Viewer scene

This article describes the navigation around the scene inside Remote Viewer on a PC. Two objects are relevant for navigating the scene:Camera: virtual...
Knowledge Center icon_circle Digital Twin
176 0 0

2026-05-26 01:07 AM

Kasper.Vestrup
Kasper.Vestrup Explorer

Advanced Physics Dynamics

IntroductionThe current implementation of the Physics Engine in Experior 7 presents difficulties in accurately simulating the dynamics of loads under ...
Knowledge Center icon_circle Digital Twin
354 0 0

2026-01-30 05:38 AM

Kasper.Vestrup
Kasper.Vestrup Explorer

Experior 7 - API

Due to our move from a self hosted webpage to the following community structure, the API documentation is now available as static html files you need ...
Knowledge Center icon_circle Digital Twin
408 0 0

2026-01-15 06:21 AM

Kasper.Vestrup
Kasper.Vestrup Explorer

Build a Controller

Step 1: Make a C# project where the main class extends the Experior.Core.Controller or Experior.Core.Logic class.Experior.Core.Controller is for makin...
Knowledge Center icon_circle Digital Twin
267 0 0

2026-01-15 05:59 AM

Kasper.Vestrup
Kasper.Vestrup Explorer

Custom connection

It is possible to extend the functionality of Experior with custom communication protocols. This is done by creating your own plugin and extending Exp...
Knowledge Center icon_circle Digital Twin
267 0 0

2026-01-15 05:57 AM

Kasper.Vestrup
Kasper.Vestrup Explorer

Load class

Loads in Experior are used to model pallets, boxes, bags, that are transported by material handling equipment like conveyors and lifts. The main names...
Knowledge Center icon_circle Digital Twin
190 0 0

2026-01-15 05:55 AM

Kasper.Vestrup
Kasper.Vestrup Explorer

ActionPoint class

Action Points are points on a Route where a load can stop and stay. They are used internally by Experior as vertices or nodes in the routing graph (wh...
Knowledge Center icon_circle Digital Twin
112 0 0

2026-01-15 05:48 AM

Kasper.Vestrup
Kasper.Vestrup Explorer

Extending the GUI with a Plugin

A plugin can be used to add custom functionality to Experior and you can also use it to extend the GUI by adding menu items and/or adding your own for...
Knowledge Center icon_circle Digital Twin
142 0 0

2026-01-15 05:47 AM

Kasper.Vestrup
Kasper.Vestrup Explorer

Rigid Sensor Part

RigidSensorPartThe class Experior.Core.Parts.Sensors.RigidSensorPart derives from the abstract class Experior.Core.Parts.RigidPart.RigidSensorPart obj...
Knowledge Center icon_circle Digital Twin
160 0 0

2026-01-15 05:43 AM

Kasper.Vestrup
Kasper.Vestrup Explorer

Interaction with Excel files

Experior provides some methods to read data from an Excel file and to write data into an Excel file. To do this you can use the Experior.Core.Data.Exc...
Knowledge Center icon_circle Digital Twin
158 0 0

2026-01-15 05:42 AM

Activity Feed
  • Posted Experior & Remote Viewer – OpenID Connect (OIDC) Login Guide on Digital Twin. ‎2026-05-26 02:06 AM
  • Posted Navigating Remote Viewer scene on Digital Twin. ‎2026-05-26 01:07 AM
  • Posted Advanced Physics Dynamics on Digital Twin. ‎2026-01-30 05:38 AM
  • Got a Like for ABB RobotStudio. ‎2026-01-28 12:47 AM
  • Got a Like for Setting up URSim with Experior 6. ‎2026-01-28 12:41 AM
  • Posted Experior 7 - API on Digital Twin. ‎2026-01-15 06:21 AM
  • Posted Build a Controller on Digital Twin. ‎2026-01-15 05:59 AM
  • Posted Custom connection on Digital Twin. ‎2026-01-15 05:57 AM
  • Posted Load class on Digital Twin. ‎2026-01-15 05:55 AM
  • Posted ActionPoint class on Digital Twin. ‎2026-01-15 05:48 AM
  • Posted Extending the GUI with a Plugin on Digital Twin. ‎2026-01-15 05:47 AM
  • Posted Rigid Sensor Part on Digital Twin. ‎2026-01-15 05:43 AM
  • Posted Interaction with Excel files on Digital Twin. ‎2026-01-15 05:42 AM
  • Posted RigidPart on Digital Twin. ‎2026-01-15 05:41 AM
  • Posted Open Office XML on Digital Twin. ‎2026-01-15 05:39 AM
  • Posted Internal communication on Digital Twin. ‎2026-01-15 05:37 AM
  • Posted Dynamic Properties on Digital Twin. ‎2026-01-15 05:36 AM
  • Posted Reports – create custom class on Digital Twin. ‎2026-01-15 05:35 AM
  • Posted Thread safe methods in Experior on Digital Twin. ‎2026-01-15 05:34 AM
  • Posted Route class on Digital Twin. ‎2026-01-15 01:02 AM
Please add bookmarks
Please subscribe to content
No drafts saved for posts
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.