EcoStruxure SEAL Forum

This forum is for engineers working EcoStruxure Building Operation, wanting to leverage the SEAL application to improve the efficiency in the engineering process.
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
  • EcoStruxure Building
  • EcoStruxure SEAL Forum
  • Label: Feature Request
Options
  • Mark all as New
  • Mark all as Read
  • Float this item to the top
  • Subscribe
  • Bookmark
  • Invite a Friend
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Label: "feature request"

View in: "EcoStruxure SEAL Forum" | Community

2 Posts | First Used: 2025-02-13

Top Labels
Top Labels
  • Alphabetical
  • Script 58
  • Design 30
  • Swedish 21
  • Announcements 14
  • Finnish 10
  • SEAL 9
  • Dwg2Tgml 8
  • Shared Scripts 7
  • Danish 5
  • Training 4
  • Norwegian 4
  • Issue 4
  • Template Library 2
  • Help 2
  • Feature Request 2
  • EFO 1
  • Multi binder 1
  • SWVersion 1
  • Graphics 1
  • MTZ02 Integration 1
  • Application Programming 1
  • Setup 1
  • Connectivity 1
  • IO Bus 1
  • Trends 1
  • Binding 1
  • Alarms 1
  • Bacnet 1
  • Modbus 1
  • PCT 1
  • error 1
  • Previous
  • 1 of 4
  • Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

EcoStruxure SEAL Forum

  • All
  • Solved
  • Unsolved
  • Unanswered
Informational
Benji
/html/rank_icons/Khan_20x20.png Benji /html/rank_icons/ADMIN-role_red.png

Welcome to the SEAL Community

SEAL is a toolbox with a number of powerful utilities to help automate and ease tasks that are usually cumbersome and time consuming. It comes with an easy to use DWG to TGML converter, and a versatile...
EcoStruxure Building icon_circle EcoStruxure SEAL Forum
11795 17 63
Latest Reply: KevinC.232

Solved
Chris_Vasiliou
/html/rank_icons/Lieutenant_JG.png Chris_Vasiliou /html/rank_icons/SE-Employee.png

Feature Expansion request - Installed Base Capture of more legacy devi...

The Installed Base Capture script looks like it will be very helpful for us. Is there any roadmap to expand the functionality to also capture other legacy Device types including INet, Continuum, Sigma ...
EcoStruxure Building icon_circle EcoStruxure SEAL Forum
910 0 3
Latest Reply: Chris_Vasiliou

Informational
Thronborg
/html/rank_icons/Lieutenant_JG.png Thronborg /html/rank_icons/SE-Employee.png

Feature request - Change default password in SEAL

It would be nice if I could change a EcoStruxure-server default password when connecting to a server.My usecase: I start PCT EBO servers. I have to connect to them via WorkStation first and change pass...
EcoStruxure Building icon_circle EcoStruxure SEAL Forum
502 1 2
Latest Reply: Benji
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.