Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84247members
353346posts

LR64 (24 GHz)

Schneider Electric
LR64 (24 GHz)
The new LR64 and LR65 from Schneider Electric offer customers the benefit of reliable, trouble free solids level measurement. Following an easy start-up procedure, the radars use powerful Frequency Modulated Continuous Wave (FMCW) radar technology and advanced signal processing and algorithms to maintain accuracy. A rugged design allows both models to be used in applications featuring: product buildup, sloping material, uneven surfaces, “rat-holes” and other challenges.
Schneider Electric
LR64 (24 GHz)
The new LR64 and LR65 from Schneider Electric offer customers the benefit of reliable, trouble free solids level measurement. Following an easy start-up procedure, the radars use powerful Frequency Modulated Continuous Wave (FMCW) radar technology and advanced signal processing and algorithms to maintain accuracy. A rugged design allows both models to be used in applications featuring: product buildup, sloping material, uneven surfaces, “rat-holes” and other challenges.
Related Posts