Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84790members
354239posts

Altivar Softstarter

Schneider Electric
Altivar Softstarter
Altivar Soft Starters provide a slow ramp-up of the motor to help decrease mechanical shock and electrical peak demand. Altivar Soft Starter is the best in class, feature-rich, easy-to-use, compact and robust Soft Starter with functionalities including torque control, communication for automation and monitoring systems. Altivar Soft Starters range from 3 A (0.37 kW) to 1200 A (900 kW) and can be used widely for any commercial and industrial application.
Schneider Electric
Altivar Softstarter
Altivar Soft Starters provide a slow ramp-up of the motor to help decrease mechanical shock and electrical peak demand. Altivar Soft Starter is the best in class, feature-rich, easy-to-use, compact and robust Soft Starter with functionalities including torque control, communication for automation and monitoring systems. Altivar Soft Starters range from 3 A (0.37 kW) to 1200 A (900 kW) and can be used widely for any commercial and industrial application.
Sort by:
Sort by:

No content available