Hospital upgrades seamlessly to comprehensive alarm notification software interfaced with their BMS
Success Stories Corner
Have a sustainability or efficiency problem? Learn how Schneider Electric is using an ecosystem approach around EcoStruxure to solve customer problems.
Auto-suggest helps you quickly narrow down your search results by suggesting possible matches as you type.
Showing results for
Show only
|
Search instead for
Did you mean:
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
2021-06-0209:00 PM
Hospital upgrades seamlessly to comprehensive alarm notification software interfaced with their BMS
Originally published on Success Stories Corner by mike_meirovitz | June 03, 2021 06:00 AM
Our Technology Partner
Our EcoXpert Partner
Customer challenge
A 900-bed Hospital in Quebec, Canada with:
Obsolete alarming software incompatible with OS
Lack of technical support
Inefficient manual alarm creation: alarms needed to be created twice, once in Building Automation System (BAS) and once in alarming software
In the customer’s words:
"We had an old alarming software that was receiving the alarms from our BAS system and sending them to various person based on a set of rules and schedule that was obsolete and needed to be replaced. The software was running on Windows XP, not compatible with Windows 10, no technical support, and the process of creating the alarms was done manually. To add a new alarm, we had to create it twice: in the BAS system and then in our alarming software. One feature that was missing and we were looking for was the ability to send text and email messages."
"Procetech-Automation and Control See came up with a solution – UCME-SmartConnector that replaced our old system. Using UCME-SmartConnector, our alarm system is now up to date. UCME-SmartConnector was addressing many of our concerns:
Supporting the latest Windows versions
Interfacing directly with Schneider Electric's EBO to capture all our alarms
The ability to send voice, text, and email messages upon receiving an alarm
Efficient and secure two-way communication with technicians and field engineers
Creating and managing our alarm based on a set of rules and be able to have a history log
After start using UCME-SmartConnector, we realized that the software was missing few features that we needed. Control See and Procetech was there to support us and developed the missing features that were added to the product. In no time the software was working perfectly.”
Customer Benefits
By using Control See’s pre-validated UCME-SmartConnector – which utilizes Schneider Electric’s SmartConnector framework – both the customer and the system integrator benefited from:
A fast engineering & implementation phase
A reliable interface between EBO and the alarm notification system
A scalable solution that can easily handle thousands of EBO alarms
End-User Testimonial
“Overall, the integration with Schneider EBO is simple. When a new alarm is created it is easy to upload it into UCME-SmartConnector. The system is much more reliable compared to our old software and the technical support is always available when required."Philippe Boudreault, Chicoutimi Hospital.