Welcome to the new Schneider Electric Community

It's your place to connect with experts and peers, get continuous support, and share knowledge.

Close
Important Announcement: WELCOME to the new Schneider Electric Community! Community is now no longer part of Exchange, and is now rebranded under se.com. If you have any bookmarks and links saved, we request you to update them to ensure that you continue accessing our community from this new location. For any issues that you might encounter as part of this change, please reach out to SchneiderCommunity.Support@se.com, and the team will help to get your issues resolved.
Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
82489members
350074posts

Need help with schneider plc

SmartConnector Forum

Discussion of SmartConnector applications for integration of various other building management systems (BMS) into EcoStruxure Building Operation

metanbeky
Cadet
0 Likes
1
276

Need help with schneider plc

Hello I'm using schneider plc TM200CE24U I'm communication it with Ethernet. The data is coming via modbus tcp/IP. Can someone please help me to program it. I mean I don't know how my modbus data is converted into input. My program is very simple I have one modbus address and when it turn zero to 1 my output should start. And when it again it turn to zero it should turn off output. Can someone please help me with it. Thank you.

Tags (1)
1 Reply 1
MaximeLaudren
Ensign Ensign
Ensign
0 Likes
0
120

Re: Need help with schneider plc

Hello Metan,

 

This forum is related to question about the smartconnector application.

For further question, I would advice to to check in the PLC forum: https://community.exchange.se.com/t5/Industrial-Automation/ct-p/industry_automation_control

 

 

To program you PLC you will need this application: EcoStruxure Machine Expert-Basic (Version V1.2)

https://www.se.com/in/en/product-range/62882-modicon-easy-m200/?parent-subcategory-id=3910&filter=bu...

 

Max

Tags (1)