Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Can't read from server. It may not have the appropriate access-control-origin settings.

SmartConnector Forum

Schneider Electric support forum for SmartConnector Framework - enabling custom integrations with EcoStruxure Building Operation, Power Monitoring Expert, and Power Operation.
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
  • EcoStruxure Building
  • SmartConnector
  • SmartConnector Forum
  • Can't read from server. It may not have the appropriate access-control-origin settings.
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
JeffBowman
JeffBowman Champion
171
KarimHussain
KarimHussain Champion
60
ardak
ardak Leader
57
View All

Recommended Forums

  • Intelligent Devices Forum

  • Metering & Power Quality

  • EcoStruxure IT Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to SmartConnector Forum
Start a Topic
dhancock_airmas
dhancock_airmas
Explorer

Posted: ‎2019-03-26 04:44 PM

0 Likes
3
1964
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
‎2019-03-26 04:44 PM

Can't read from server. It may not have the appropriate access-control-origin settings.

Hi,

 

I have installed the SmartConnector on my EBO Server for Bueno Analytics to accesss, the SmartConnector is working and accessing the database from the local network. When we try a remote connection we get the web page display with "Can't read from server. It may not have the appropriate access-control-origin settings." error. 

 

Using Chorme  this error is shown in the developer tool console "Access to XMLHttpRequest at 'http://192.168.2.9:8083/swagger/docs/v1' from origin 'http://165.228.3.48:8083' has been blocked by CORS policy: No 'Access-Control-Allow-Origin' header is present on the requested resource."

 

I am using EBO 2.0.3.45 on a Windows 2016 Server, SmartConnector 2.4.17, the ADSL & Windows firewalls are off. Have I missed something in the setup of the software or do I have to add Access-Control-Allow-Origin to one of the files installed.

 

Regards,

 

Dale

Attachments
SmartConnector Error.docx
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 3
JeffBowman
JeffBowman Champion
Champion

Posted: ‎2019-03-27 05:14 AM

0 Likes
2
1960
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
‎2019-03-27 05:14 AM

Hi Dale,

 

If you try and set where the IP is 192.168.2.9:8083 to 165.228.3.48:8083 does it work?

 

Also, even though the swagger page isn't loading correctly, the simple fact you can access the page shows that in general the Framework is setup correctly. The real test would be to point Bueno Analytics at this endpoint to make sure it is working.

 

Regards,

 

-Jeff

Reply
dhancock_airmas
dhancock_airmas
Explorer

Posted: ‎2019-04-04 08:02 PM

0 Likes
1
1955
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
‎2019-04-04 08:02 PM

Jeff,

 

We have tried changing the IP address and you cannot log in to access the data. When you try to log in you get a pop up that has 165.228.3.48:8083 says with nothing else. (Please see attached)

 

Regards,

 

Dale

Attachments
SmartConnector Login Error.docx
Reply
JeffBowman
JeffBowman Champion
Champion

Posted: ‎2019-04-05 06:49 AM

0 Likes
0
1951
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
‎2019-04-05 06:49 AM

Hi Dale,

 

The issue you came across is unfortunetly a likely bug on our side. I am gonna guess that you have it setup so that your endpoint address is configured as 'http://+:8083', and that you are connecting to this webpage from a different machine than where Smart Connector is installed. The bug if in this scenario, we are trying to authenticate using 127.0.0.1 as the IP address of the server, which of course in this case is not correct at all, and it should be using 165.228.3.48. Hence the error you are seeing.

 

The workaround for this would be set the endpoint address as http://165.228.3.48 (assuming this is not a DMZ address) or you can log into this swagger page from the machine where Smart Connector is installed. In the mean time, I am have been looking into a fix, and it is of course a bit more complicated then I would have liked.. So I am not sure when this will be available. 

 

The above said, it is only Swagger that is the issue and not the REST endpoint itself. If you were to use another REST client (either code based, or something like Postman) to send requests. It would work as expected.

 

Best Regards,

 

-Jeff
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.