Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84783members
354229posts

Wiser App - removing the IPC outdoor

Schneider Electric Wiser Forum

Connect with Wiser Smart Home solution experts in the Schneider Electric Wiser forum. Discuss tips on features, updates, installation, and how to get the most out of your Wiser products.

Solved
Esperanto
Lieutenant JG
Lieutenant JG
0 Likes
1
218

Wiser App - removing the IPC outdoor

Hello, how can I remove my IPC outdoor with the wiser App?

Tags (1)

Accepted Solutions
Alfred_SE
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
215

Re: Wiser App - removing the IPC outdoor

Hello! Thanks for reaching.

Using the Wiser app, you can remove a device from the device list.

Follow the steps to remove the device:

  1. On the Home page, tap All devices > IP Camera Outdoor.
  2. Tap the pen icon and tap Settings.
  3. Tap Remove device (A) and tap Confirm

TIP: Alternatively, you can long tap on the IP Camera Outdoor on the home page to remove the device.

NOTE: Removing the device will reset the device. The LED starts blinking red indicating that the device is ready to pair with another network

Capture.PNG

Alfred Francis

See Answer In Context

Tags (1)
1 Reply 1
Alfred_SE
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
216

Re: Wiser App - removing the IPC outdoor

Hello! Thanks for reaching.

Using the Wiser app, you can remove a device from the device list.

Follow the steps to remove the device:

  1. On the Home page, tap All devices > IP Camera Outdoor.
  2. Tap the pen icon and tap Settings.
  3. Tap Remove device (A) and tap Confirm

TIP: Alternatively, you can long tap on the IP Camera Outdoor on the home page to remove the device.

NOTE: Removing the device will reset the device. The LED starts blinking red indicating that the device is ready to pair with another network

Capture.PNG

Alfred Francis
Tags (1)