Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84761members
354191posts

Upgrade from Scadapack 300 series to 400/500 series

Remote Operations Forum

Collaborate and share knowledge on the extensive range of remote systems and devices, including SCADA radios and RTUs, on the Schneider Electric Exchange Remote Operations (formerly SCADA & Telemetry) forum. From commissioning SCADA integration devices and software, to enhancing existing installations or troubleshooting, connect with a global community of experts and users. Subscribe today.

Solved
SG_Elsis_TS
Crewman
Crewman
7
1779

Upgrade from Scadapack 300 series to 400/500 series

Our company has been working with Scadapack 300 series for 20+ years. Now, that new series are available, I would like to ask a few relevant questions, regarding the functionality of the new series Scadapacks:

 

  1. Will there be any support for C/C++ programming? A significant part of programming in our field is done using C/C++, therefore Scadapack 400/500 series compatibility for this feature is essential. So far, I haven't seen any mentions of this.
  2. Having read the documentation, the majority of the old functions/function blocks have been saved in one way or another. Although, there are two functions that we use extensively in Scadapack 300 series: DLOG and GETL. I see, that DLOG function will be supported in the future releases but GETL function will not be supported. Will the functionality of these two functions be continued? Or will one function be extended to represent both of the old ones?

Accepted Solutions
Joel_Weder
Commander Commander
Commander
4
1751

Re: Upgrade from Scadapack 300 series to 400/500 series

From our SCADAPack Product Manager:

 

1) Will x70 support C or C++ programming? 

"Yes, this will be included as one of the capabilities of the SCADAPack 470i and 474i with the Linux board. I expect it will be released no later than the end of 2021."

 

2) How about the GETL (get log) function block? 

"Yes, we are developing a new integrated logging function which will include a similar function to GETL in a future RemoteConnect release."

Joel Weder
Remote Operations Specialist
Schneider Electric

See Answer In Context

7 Replies 7
AlastairF
Lieutenant Lieutenant
Lieutenant
6
1769

Re: Upgrade from Scadapack 300 series to 400/500 series

1. Support for C++/C# and other languages (Python etc) will be coming with the SCADAPack470i

 

2. A version of the DLOG_F function is provided in the SCADAPack x70 Extensions Library v2.2 that are available free of charge via Exchange.

https://shop.exchange.se.com/en-US/apps/76149/scadapack-x70-extensions-library-for-remoteconnect

 

SG_Elsis_TS
Crewman
Crewman
0 Likes
5
1761

Re: Upgrade from Scadapack 300 series to 400/500 series

Thank you for your reply!

 

I didn't know about Scadapack 470i version, thank you. 

 

I saw the DLOG_F function in the documentation provided with the Remote Connect software, though my question was about DLOG function. It records data entries in the data log internally and not to a separate file. It is stated in the documentation, that this function will be supported in later releases and GETL, which is used to extract the data records from the data log, will not be supported. So the question is - will these two functions remain in the new series? And if so, will they retain the same functionality?

Joel_Weder
Commander Commander
Commander
4
1752

Re: Upgrade from Scadapack 300 series to 400/500 series

From our SCADAPack Product Manager:

 

1) Will x70 support C or C++ programming? 

"Yes, this will be included as one of the capabilities of the SCADAPack 470i and 474i with the Linux board. I expect it will be released no later than the end of 2021."

 

2) How about the GETL (get log) function block? 

"Yes, we are developing a new integrated logging function which will include a similar function to GETL in a future RemoteConnect release."

Joel Weder
Remote Operations Specialist
Schneider Electric
Abzeles
Crewman
Crewman
0 Likes
3
1089

Re: Upgrade from Scadapack 300 series to 400/500 series

Hello,

 

I'm curious when Schneider are planning to release update for x70 RTU controllers to support C/C++ language?

 

You mentioned below that it will be release at the end of 2021, but as much as I know it's not released yet.

 

Regards,


 

Joel_Weder
Commander Commander
Commander
0 Likes
2
1077

Re: Upgrade from Scadapack 300 series to 400/500 series

Hi Jonas,

 

I've received new  information about the addition of C language capability into x70 SCADAPacks. Rather than add ability to run just C (or C++) apps within all x70 models, the plan is to offer our new SCADAPack 470i and 474i models. These will include a second processor board with a Linux operating system. (as well as more LAN and USB ports) This will allow the user to load and run applications written with C, Python or Node-RED logic.

 

The 470i and 474i models should be available by September. Note however that if you have any existing 470 or 474 models, they unfortunately cannot be upgraded to the "i" version.

 

Joel Weder

Joel Weder
Remote Operations Specialist
Schneider Electric
Abzeles
Crewman
Crewman
0 Likes
1
1063

Re: Upgrade from Scadapack 300 series to 400/500 series

Thank you for the information. That's a good news.

 

Maybe there is a possibility to get a characteristics for these controllers ? 

 

Regards, 

Jonas

Joel_Weder
Commander Commander
Commander
0 Likes
0
1013

Re: Upgrade from Scadapack 300 series to 400/500 series

Hello Jonas & all,

 

Here is a DRAFT version of the datasheet for the SCADAPack 470i and 474i. It is very similar to the 470 and 474, but adds the Linux board. Also an informational sheet about features of these new models.

 

Note that because these are draft documents, some specifications may change before the products are released.

 

Joel Weder
Remote Operations Specialist
Schneider Electric
Attachments