Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Hello All,
I understand that HU280 CPU hold the protocol buffer events in case of SCADA connection failure initially and thereafter power loss/reboot.
However, I would like to know maximum number of events stored in buffer memory per open standard telemetry protocol such as: IEC 61850, IEC 101, IEC 104 and DNP3.
Link copied. Please paste this link to share this article on your social media post.
Hello @DhananjayJamdade
For IEC 61850
Each buffered RCB instance has two circular buffers of 20 kB:
Beware: configurable buffer size is not supported.
How many events can be buffered in 20kB?
To calculate how many events this equates to, we need to consider specific DO types. For example, one SPS DO event in a typical status dataset of 64 SPS DOs. Each entry in the RCB buffer stores:
Therefore a server side BRCB buffer could store approximately 20kB / 42 = 487 such SPS events
For DNP3.0 slave
Buffer size could be configured in Easergy Builder for every Object type like here below:
For IEC 101-104 slave
Buffer size could be configured in Easergy Builder for every point type like here below:
Link copied. Please paste this link to share this article on your social media post.
Thank you
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.