Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PowerLogic T300 - Is it possible to use T300-ATS for 3 MV sources?

Protection & Control

Schneider Electric support forum about Protection Relays, Substation Controllers & RTUs, Arc Flash Devices & Systems in Medium Voltage and Low Voltage. A place to get support on product selection, installation, commissioning and troubleshooting.
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
  • EcoStruxure Power & Grid
  • Protection & Control
  • PowerLogic T300 - Is it possible to use T300-ATS for 3 MV sources?
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Araceli_Monje
Araceli_Monje Mentor
74
JuanRayo
JuanRayo Mentor
41
Arun-kumar_PS
Arun-kumar_PS Mentor
33
View All

Recommended Forums

  • Metering & Power Quality

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Protection & Control
Start a Topic
Solved
med
med
Explorer

Posted: ‎2025-11-17 02:34 PM . Last Modified: ‎2026-01-16 02:47 AM

0 Likes
3
616
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
‎2025-11-17 02:34 PM

PowerLogic T300 - Is it possible to use T300-ATS for 3 MV sources?

Hello everyone,
I’m working on configuring a 3-source ATS using a Schneider PA T300, and I’m not sure which method is required.

Can this logic (source selection, priority, switching commands, interlocks) be done only with formulas inside Easergy Builder, or do I need to use ISaGRAF / FBD to build the control sequence?

If someone has already managed a 3-source ATS on a T300, which approach do you recommend, and why?

Thanks for your help!

Labels
  • Labels:
  • Application cases
  • PowerLogic T300
Tags (4)
  • Tags:
  • english
  • PowerLogic T300
  • t300
  • T300 ATS
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Mathieu_Lansoy
Mathieu_Lansoy Mentor
Mentor

Posted: ‎2026-01-14 08:47 AM

1 Like
0
478
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
‎2026-01-14 08:47 AM

Hello,

 

This kind of solution can be better developped with an ISaGRAF program. This is more efficient to manage sequences, loops and timers than the formulas, and adapted to "PLC programming" thinking (if you know FBD language for example).

you can find examples of programs done for a 2-source ATS on the T300_sharepoint and rework them.

 

regards,

 

  Mathieu.

See Answer In Context

Reply
Replies 3
Araceli_Monje
Araceli_Monje Mentor
Mentor

Posted: ‎2026-01-14 06:22 AM

0 Likes
0
484
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
‎2026-01-14 06:22 AM

@Mathieu_Lansoy , could you please support @med with his question?, thanks.

Reply
Mathieu_Lansoy
Mathieu_Lansoy Mentor
Mentor

Posted: ‎2026-01-14 08:47 AM

1 Like
0
479
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
‎2026-01-14 08:47 AM

Hello,

 

This kind of solution can be better developped with an ISaGRAF program. This is more efficient to manage sequences, loops and timers than the formulas, and adapted to "PLC programming" thinking (if you know FBD language for example).

you can find examples of programs done for a 2-source ATS on the T300_sharepoint and rework them.

 

regards,

 

  Mathieu.

Reply
JYPOC
JYPOC Mentor
Mentor

Posted: ‎2026-01-16 02:58 AM

0 Likes
0
459
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
‎2026-01-16 02:58 AM

Hello Med,

T300 ATS algorithms that are provided free of charge (whether in T300 firmware or as ISAGRAF ready-made programs) are for 2 MV sources:

  1. Auto-Change Over (between 2 MV lines),
  2. GENerator (between a MV line and a GENSET)
  3. Bus Tie Automatism (between 2 MV lines and with a coupling MV switch)

As Mathieu explained, you can develop your own ATS system (for example, with 3 MV sources). For that, you need to purchase an ISaGRAF 5.22 license from Schneider Electric to build your program.

Once your program is fully tested, you can inject it into as many T300 units as you want (the license is only required to create the program, not to use it).

BR - Jean-Yves
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.