Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84496members
353716posts

Energy efficiency: IEC 60364-8-1 and Energy Conservation Building Code (India) - Ask your questions about this comparison!

Power Distribution and Digital

Join experts & peers to learn, share and engage about the key trends of electrical distribution around safety, availability, efficiency and connectivity, as well as power standards & regulations. From design to implementation and operation, let’s discuss how digital and software are transforming your business and your day-to-day work.

Solved
AalokD
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Energy efficiency: IEC 60364-8-1 and Energy Conservation Building Code (India) - Ask your questions about this comparison!

Not yet another energy efficiency standard! 🙄

 

Over the last couple of years, a couple of important developments in the energy efficiency standards space are worth taking note of, as these will be an integral part of the vocabulary and language of professionals going forward:

  1. Energy Conservation Building Code 2017  (ECBC) was published and is in the process of being implemented in various states across the country. 
  2. IEC 60364-8-1 was adopted as  IS 16996:2018 / IEC 60364-8-1 and published by the Bureau of Indian Standards.

Staying on top of requirements across different codes and standards can be difficult. Which is why we took some time to put together this document comparing ECBC 2017 and IEC 60364-8-1:2019 for your ready reference.

 

Please let us know if you find this comparison helpful! Or if you have any questions!

 

- Aalok A. Deshmukh, LEED Fellow, CMVP

Director - Energy Efficiency


Accepted Solutions
Nedjma
Community Alumni (Retired)
Community Alumni (Retired)
0 Likes
0
1040

Re: Energy efficiency: IEC 60364-8-1 and Energy Conservation Building Code (India) - Ask your questions about this comparison!

Hello @AalokD,

 

Thanks for sharing this useful information.🙂

 

 

 

 

See Answer In Context

Tags (1)
1 Reply 1
Nedjma
Community Alumni (Retired)
Community Alumni (Retired)
0 Likes
0
1041

Re: Energy efficiency: IEC 60364-8-1 and Energy Conservation Building Code (India) - Ask your questions about this comparison!

Hello @AalokD,

 

Thanks for sharing this useful information.🙂

 

 

 

 

Tags (1)