Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84600members
353871posts

MODBUS TCP on optic fiber with M340

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.

joaomoreira123
Cadet
0 Likes
1
491

MODBUS TCP on optic fiber with M340

Hello,

 

I'd like to ask for a technical confirmation on using MODBUS TCP in a M340 + Fiber Converter Card (BMXNRP0200C) or Switch (ADAM 6521) + Fiber Optic patch cords and cable topology to communicate with a SCADA system.

 

The main objective is to provide a fiber optic connection point inside a control panel because it is located in a area prone to electrical interference. The protocol to be used would be MODBUS TCP. We have two simple topologies in mind but we are not sure if they are feasible. So i'm asking for a little support about it.

 

Considering the following simplified topologies, am I able to use MODBUS TCP to communicate from the M340 to the SCADA workstation with no problem? I'm not sure if the protocol allows this kind of change on the physical medium like if it was pure Ethernet.

Simplified TopologiesSimplified Topologies

 

Tags (1)
1 Reply 1
trowe
Crewman
Crewman
0 Likes
0
465

Re: MODBUS TCP on optic fiber with M340

Provided none of the convertors block TCP port 502 the transfer of Modbus/TCP will be oblivious to the fact it is changing medium.

 

I have used the ADAM units before without issue

Tags (1)