Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

M580 to M580 - PLC Communications/Data Exchange

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
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
  • Industrial Automation
  • Modicon PAC Forum
  • M580 to M580 - PLC Communications/Data Exchange
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Trinxs1
Trinxs1 Leader
19
YONGHO-KIM
YONGHO-KIM Mentor
10
ciupol
ciupol
9
View All

Recommended Forums

  • Industry Automation and Control Forum

  • Machine and Motion Control Forum

  • Alliance Partner Program System Integrator

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Modicon PAC Forum
Start a Topic
Taffy123
Taffy123
Explorer

Posted: ‎2024-07-09 02:22 AM . Last Modified: ‎2024-07-09 02:27 AM

0 Likes
1
2820
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
Posted: ‎2024-07-09 02:22 AM . Last Modified: ‎2024-07-09 02:27 AM

M580 to M580 - PLC Communications/Data Exchange

Hi all,

 

Pretty new to using Schneider currently I'm trying to get communications working between two M580 PLCs.

 

One of the M580s is just being used as a glorified RIO with no real code inside of it, just passing all IO back to the mainM580 processor (this was done due to hardware constraints by the client).

 

The Main M580 PLC processor is a BMEP583020 and we have a NOC0301 that is connected to the RIO M580 CPU ethernet ports. The RIO M580 is a BMEP583020.

 

The code has been written attempting to use READ_REMOTE to try and read data between each of these PLCs but I am constantly getting an error which is just a generic error (1100). I'm using the ADDMX block to set the address for the READ_REMOTE block - which is 0.3.0{10.80.64.139} for the Main PLC trying to read the RIO PLC data from the NOC unit.

 

The issue is being unfamiliar with the Schneider, and having not written the code, I'm not even sure the READ_REMOTE is the correct way to facilitate communications and if it is what's going wrong. 

Attachments
Labels
  • Labels:
  • 02. Modicon M580 ePAC
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
Trinxs1
Trinxs1 Leader
Leader

Posted: ‎2024-09-18 09:01 PM

0 Likes
0
2613
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
Posted: ‎2024-09-18 09:01 PM

A few considerations:

  1. Is the data dictionary enabled and operating in the target PLC?
  2. Is the name of the target variable or variables added as a string and is identical to the variable in the target PLC.  As a note, I use the same variable name in the source PLC but add a reference or comment to indicate the variable is sourced or used in another PLC.
  3. Please make sure the address is entered as a string for the ADDMX block.
  4. Please also check that the network is OK and that you can ping the target the PLC when connected to the service port of the NOC module.
  5.  

 

Trinxs
Senior Technical Sales Consultant - PAC
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.