Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.
Search in
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-09-04 11:09 PM
Dear,
I have one project to let SCADA can communication with PLC M580 by protocol IEC104. So I will use the module BMXNOR2200H for this communication but I do not know who to configure.
Thanks
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-09-11 12:43 AM
Hi Sophearak KAO,
Kindly check the attached file. It's a sample video using the BMENOR2200H module with only serial ports. One module is configured with IEC 101 Master, and another one is IEC 101 Slave.
The video gives you a rough idea of how to configure the ASDU common address and add the IOA Addressing points on both sides, Master and Slave.
In your case, you are using IEC 104, so you should have Server and Client configurations. However, the configuration is almost the same.
It seems like you are making the BMENOR2200H module act as an IEC 104 server, and Scada should be the IEC 104 client.
You can use the tool suggested by Trinxs and configure it as an IEC 104 Client. Alternatively, you can download the TestHarness tool from TMW and use the trial version.
NOTE: You might have to create an account on their website first.
TMW Product Downloads (trianglemicroworks.com)
I hope the shared video helps you configure the client and server properly with the proper ASDU address and IOA addressing point on both client and server and that you are able to exchange information between them. If you are still facing issues, please share your ECE application in *.sta format.
NOTE: The shared demo video contains just the basic configuration for the sake of exchange between client and server, but the IEC 104 client/server configuration should be done based on the customer's application and requirements, which requires a basic understanding of the protocol itself.
Best Regards,
MWS
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-09-06 12:11 AM
First of all which version of the module do you have?
The following links will help with the configuration..
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-09-08 08:26 PM
The module itself once configured will use the nominated protocol. You may need to have additional software for two different parts of this.
1. software to configure the device you wish to communicate with. This will depend on the device.
2. sometimes simulation software can be very useful. IEC 104 Client Master Simulator tool download | SourceForge.net is one example I was able to find that can be used as a client if the NOR module is a server. Alternatively google can provide other simulators that can act as an IEC 104 server.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-09-09 07:33 PM
Dear,
In the video they mention only DNP3 server but it does not have for IEC60870-5-104.
Can you share me an example or configuration file for IEC104 server ?
Thanks
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-09-11 12:43 AM
Hi Sophearak KAO,
Kindly check the attached file. It's a sample video using the BMENOR2200H module with only serial ports. One module is configured with IEC 101 Master, and another one is IEC 101 Slave.
The video gives you a rough idea of how to configure the ASDU common address and add the IOA Addressing points on both sides, Master and Slave.
In your case, you are using IEC 104, so you should have Server and Client configurations. However, the configuration is almost the same.
It seems like you are making the BMENOR2200H module act as an IEC 104 server, and Scada should be the IEC 104 client.
You can use the tool suggested by Trinxs and configure it as an IEC 104 Client. Alternatively, you can download the TestHarness tool from TMW and use the trial version.
NOTE: You might have to create an account on their website first.
TMW Product Downloads (trianglemicroworks.com)
I hope the shared video helps you configure the client and server properly with the proper ASDU address and IOA addressing point on both client and server and that you are able to exchange information between them. If you are still facing issues, please share your ECE application in *.sta format.
NOTE: The shared demo video contains just the basic configuration for the sake of exchange between client and server, but the IEC 104 client/server configuration should be done based on the customer's application and requirements, which requires a basic understanding of the protocol itself.
Best Regards,
MWS
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-09-11 04:54 AM
You are welcome. If you are still facing problems, let me know.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-09-27 01:23 AM
@Siddiqui I have try with IEC104 it does not work. Would you mind you check my configuration as atttached file.
Thanks.
Link copied. Please paste this link to share this article on your social media post.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-10-08 01:16 AM
Somehow, I missed your last post notification. I hope you manage to sort out the problem, but if you are still facing issues, check my comments below.
I checked your configuration on the client side of the BMENOR module, and it seems OK, but I would suggest doing the following.
For your reference, I shared the TMW Test Harness IEC 104 server-side sample configuration snapshots.
Best Regards,
MWS
Link copied. Please paste this link to share this article on your social media post.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.