Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84599members
353869posts

M340 M580 X80 firmware files V5.3

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.

AlastairF
Lieutenant Lieutenant
Lieutenant

M340 M580 X80 firmware files V5.3

This is a more comprehensive package of links (Firmware link spreadsheet V5.3) than the one provided with SESU.

New update as at 2021-10-05

The attached spreadsheet lists collated links to publicly available firmware for M340/ M580/ X80/ Advantys/ Connexium/ Modicon switches.

Updated with:

  • M340
  • MC80
  • BMXAMI
  • BMXNOR
  • Advantys
  • EADM

Feedback welcome (broken links, improvements or additions needed).

 

Attachments
Tags (1)
1 Reply 1
Robert_Willis
Ensign Ensign
Ensign

Re: M340 M580 X80 firmware files V5.3

Thank you for your continued support at keeping this updated.

Tags (1)