Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84398members
353586posts

network builder wizard

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

JeroenDeville
Lt. Commander Lt. Commander
Lt. Commander

network builder wizard

Dear

 

I really like the network builder wizard in ION setup.

Can it also be used when adding a new site in the network view, or in existing systems?

 

regards

 

Jeroen

1 Reply 1
Robert_Lee
Captain Captain
Captain
0 Likes
0
260

Re: network builder wizard

The network builder wizard shown to First Time users is meant to instruct these novice users on the process on how to insert sites/devices into the system (as opposed to just showing them an empty network viewer).  Most users that I know that get comfortable in how to add sites/devices using the Insert Item from the menu/toolbar usually don't need to have the wizard walk through each time.