Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Serial communication stopped on PM5560

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Serial communication stopped on PM5560
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
571
Mehran_Mehrnia
Mehran_Mehrnia Champion
203
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
Miyai
Miyai
Contributor

Posted: ‎2026-07-30 12:02 AM

0 Likes
5
277
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
‎2026-07-30 12:02 AM

Serial communication stopped on PM5560

 

Hello,

 

Are there any situations where the PM5560 stops Modbus RTU communication?

 

I was conducting Modbus RTU communication tests between a master PC and a slave PM5560 when the response from the slave suddenly stopped.

 

I sent several request commands from the master side, but there is no response from the slave side.

 

Communication returned to normal after restarting the PM5560.

PM5560 version is V4.5.0, and the communication settings are correct.

 

Is there any reason why the PM5560 units would stop communicating?

Multiple PM5560 units are connected to the serial communication circuit, and two of them experienced the same issue simultaneously.

 

Best regards,

Miyai

 

Labels
  • Labels:
  • PM5000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
akash_das
akash_das Troubleshooter
Troubleshooter

Posted: ‎2026-08-13 03:08 AM

0 Likes
0
55
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
‎2026-08-13 03:08 AM

Hi @Miyai Thanks for the update. if such issue occurs in the future please raise a support case with relevant details for our analysis. Thank you!

See Answer In Context

Reply
Replies 5
Jesus_Diaz
Jesus_Diaz Mentor
Mentor

Posted: ‎2026-07-30 12:38 PM

0 Likes
3
256
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
‎2026-07-30 12:38 PM

Hi @Miyai 

 

Under normal operation, the PM5560 should not stop responding to Modbus RTU requests. Could you please provide the following information?

 

  • What polling rate is being used?
  • What hardware are you using to communicate with the meters (for example, a USB-to-serial converter)?
  • How many registers are being read, and which registers are they?
  • How many devices are connected to the serial line? Are they all running the same firmware version and model?
  • What are the baud rate, parity, and stop-bit settings?
  • Did both PM5560 meters stop responding at exactly the same time?

Regards,
JD

Reply
Miyai
Miyai
Contributor

Posted: ‎2026-07-30 05:18 PM

0 Likes
2
248
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
‎2026-07-30 05:18 PM

Hi @Jesus_Diaz 

 

What polling rate is being used?
⇒polling rate is one per second.
What hardware are you using to communicate with the meters (for example, a USB-to-serial converter)?
⇒Ethernet-to-serial converter.
How many registers are being read, and which registers are they?
⇒Since the system belongs to the client, I don't have the full details, but it captures standard parameters such as voltage and current, involving around 16 registers.
How many devices are connected to the serial line? Are they all running the same firmware version and model?
⇒Approximately 20 devices are connected to the serial communication circuit. These include products from various manufacturers. The PM5560 units on the same circuit are running the same firmware version.

What are the baud rate, parity, and stop-bit settings?
⇒The baud rate is 9600, with 8N2 settings.
Did both PM5560 meters stop responding at exactly the same time?
⇒Communication stopped at the same time.

 

 

Only the communication function was disabled; the meter's measurement display and other functions were operating normally.

Do you know the causes of communication function freezes?

I have already contacted Schneider's quality department, but I am having trouble because I haven't received a reply.

 

Best regards,

Miyai

Reply
Jesus_Diaz
Jesus_Diaz Mentor
Mentor

Posted: ‎2026-08-04 02:51 PM

0 Likes
1
150
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
‎2026-08-04 02:51 PM

Hi @Miyai,

 

Thanks for the information.

 

Has the client tried isolating the two PM5560s to see how they behave? How long does it take for this issue to occur, and how often does it happen?

 

@rohith-s @akash_das Do you have any suggestions for this case?

Reply
Miyai
Miyai
Contributor

Posted: ‎2026-08-04 11:03 PM

0 Likes
0
136
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
‎2026-08-04 11:03 PM

Hi @Jesus_Diaz 

 

This incident occurred only once.
It is currently operating normally.
The communication interruption has not recurred.

 

 

Best regards,

Miyai

Reply
akash_das
akash_das Troubleshooter
Troubleshooter

Posted: ‎2026-08-13 03:08 AM

0 Likes
0
56
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
‎2026-08-13 03:08 AM

Hi @Miyai Thanks for the update. if such issue occurs in the future please raise a support case with relevant details for our analysis. Thank you!
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.