Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Separate kWh Accumulation Based on Power Source Using Digital Input on ION9000

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Separate kWh Accumulation Based on Power Source Using Digital Input on ION9000
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
195
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
juanpablo.vargasvillalobos
juanpablo.vargasvillalobos Explorer
Explorer

Posted: ‎2026-07-02 08:41 AM

0 Likes
3
128
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
‎2026-07-02 08:41 AM

Separate kWh Accumulation Based on Power Source Using Digital Input on ION9000

Is it possible to configure some logic in ION9000 to separately record kWh consumption based on the active power source?

For example, when the site transfers from the utility supply to the generator backup, can the meter use a digital input to detect when the generator is running and then accumulate energy (kWh) into a separate register only while that digital input is active?

In other words, I would like to have one energy register dedicated to generator operation and have it accumulate consumption only during the periods when the generator is supplying power. Has anyone implemented something similar using ION logic or digital inputs in an ION meter?

Labels
  • Labels:
  • ION Setup
  • ION9000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2026-07-02 10:01 AM . Last Modified: ‎2026-07-02 10:02 AM

0 Likes
2
123
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
‎2026-07-02 10:01 AM

Hello @juanpablo.vargasvillalobos ,

 

Can ION9000 meter do this yes. Does the meter do this by default, not really. You can make a framework that enables integrator module only when the Digital input is true. 

Getting the meter to only activate the new Integrator would be a lot more complex task.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Replies 3
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2026-07-02 10:01 AM . Last Modified: ‎2026-07-02 10:02 AM

0 Likes
2
124
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
‎2026-07-02 10:01 AM

Hello @juanpablo.vargasvillalobos ,

 

Can ION9000 meter do this yes. Does the meter do this by default, not really. You can make a framework that enables integrator module only when the Digital input is true. 

Getting the meter to only activate the new Integrator would be a lot more complex task.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Reply
juanpablo.vargasvillalobos
juanpablo.vargasvillalobos Explorer
Explorer

Posted: ‎2026-07-02 11:18 AM

0 Likes
1
120
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
‎2026-07-02 11:18 AM

Thank you very much, @charles ; I’ll look into the best way to do it.

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2026-07-06 02:36 PM

1 Like
0
75
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
‎2026-07-06 02:36 PM

Hello @juanpablo.vargasvillalobos 

In ION 9000 meters there is a concept called Conditional Energy, perhaps this can do what you are looking for.
https://product-help.se.com/docs/PowerLogic-ION9000/en-us/content/13-measurements/conditional-energy...

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.