Ask our Experts
Didn't find what you are looking for? Ask our experts!
New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
Search in
Please select a country to continue with beta search.
Link copied. Please paste this link to share this article on your social media post.
Hello,
Regarding the PM5560 firmware update (ver 2.5.x ⇒ ver 4.0.x),
please tell me about the update process.
I believe this would be an update using the firmware upgrade tool; in this case,
is it necessary to enable FTP?
Also, in the ver. 2.x.x firmware, is the initial (default) setting for FTP Enabled or Disabled?
Regard,
Okada
Link copied. Please paste this link to share this article on your social media post.
Hi @T.Okada In the user manuals, we have mentioned the pre-requisites for each of the applicable firmware upgrade methods based on firmware versions.
Please follow the pre-requisites along with steps given for upgrade.
Link copied. Please paste this link to share this article on your social media post.
Hi @T.Okada
As documented in PM5500 user guide, use the Firmware Upgrade Tool method for PM5560 from 2.5.x to 4.0.x:
FTP is required and must be enabled only when using the FTP‑server upgrade method. However, in the document 'Firmware upgrade user manual snippet.pdf' included in the latest firmware package, the section “Meter upgrade requirements for firmware upgrade tool” notes a special case that applies only to the PM5561 model. In that case, if the FTP server is disabled, it must be enabled through the meter display. This exception does not apply to the PM5560.
"Also, in the ver. 2.x.x firmware, is the initial (default) setting for FTP Enabled or Disabled?"
Best Regards,
-Mehran
L3 Expert Advanced metering
Link copied. Please paste this link to share this article on your social media post.
Hello @Mehran_Mehrnia
Thank you for your prompt reply.
I understand that I don’t need to enable the FTP setting when upgrading the PM5560 using the Firmware Upgrade Tool (from ver. 2.5.x to ver. 4.0.x).
I have one more question: do I need to enable the FTPS setting when upgrading the PM5560 using the Firmware Upgrade Tool (from ver. 4.0.x to ver. 4.x.x)?
Based on my testing, my understanding was that enabling FTPS is required when upgrading the PM5560 using the Firmware Upgrade Tool (from ver. 4.0.x to ver. 4.x.x).
Regards,
Okada
Link copied. Please paste this link to share this article on your social media post.
Hi @T.Okada,
I tested the upgrade from a 4.x.x version to another 4.x.x version with FTPS disabled. After clicking the Upload FW button, the tool automatically enabled FTPS on the meter.
Before:
After:
Please also note that you can upgrade directly from the meter’s webpages, which is easier if you are only working with a limited number of meters.
Regards,
JD
Link copied. Please paste this link to share this article on your social media post.
Hi @T.Okada In the user manuals, we have mentioned the pre-requisites for each of the applicable firmware upgrade methods based on firmware versions.
Please follow the pre-requisites along with steps given for upgrade.
You’ve reached the end of your document
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.