Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PQA1 Vavg Sliding Ref Voltage

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • PQA1 Vavg Sliding Ref Voltage
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
566
Mehran_Mehrnia
Mehran_Mehrnia Champion
194
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Related Products
product field
Schneider Electric
Power Monitoring Expert

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
Dusica
Dusica
Contributor

Posted: ‎2025-12-17 12:04 AM

0 Likes
3
431
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
‎2025-12-17 12:04 AM

PQA1 Vavg Sliding Ref Voltage

Hello all, 

Is there any documentation and explanation how is "PQA1 Vavg Sliding
Ref Voltage" value calculated in the Burst data (Sag/swell Log)? 

 

Best regards, 
Dušica

  • Thumbnail of Power Monitoring Expert
    Schneider Electric
    Power Monitoring Expert
View products (1)
Labels
  • Labels:
  • ION Setup
  • ION9000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-12-19 08:55 AM

1 Like
2
427
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
‎2025-12-19 08:55 AM

Hi @Dusica 

 

As mentioned in ION Reference -> Power Quality Aggregator Module, the Power Quality Aggregator Module complies with some sections of the IEC 61000-4-30 standard, which requires tracking voltage variations relative to a "sliding" or "moving" average rather than just a fixed nominal value which continuously computes RMS voltage values every half-cycle and aggregates these RMS values over defined intervals (e.g., 150/180 cycles, 10 sec, 10 min, 2 hr).

 

During an event, burst data logs the instantaneous voltage alongside the Vavg Sliding Ref Voltage. If the RMS voltage deviates from this baseline beyond configured thresholds (sag <90%, swell >110%), the event is flagged. The sliding reference ensures thresholds adapt to long-term changes in supply voltage, avoiding false positives.

 

For more information, please refer to standard IEC 61000-4-30 section 5.4.4 which pertains to the measurement methods for the duration of supply voltage dips and swells and defines the criteria for when an event begins and ends.

 

In the following technical note, you will find more information about the compliance of meters with the IEC 61000-4-30 (4-30) standard:
IEC 61000-4-30 compliance and ION meters

 

Best Regards,

-Mehran

L3 Expert Advanced metering

See Answer In Context

Reply
Replies 3
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2025-12-19 08:55 AM

1 Like
2
428
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
‎2025-12-19 08:55 AM

Hi @Dusica 

 

As mentioned in ION Reference -> Power Quality Aggregator Module, the Power Quality Aggregator Module complies with some sections of the IEC 61000-4-30 standard, which requires tracking voltage variations relative to a "sliding" or "moving" average rather than just a fixed nominal value which continuously computes RMS voltage values every half-cycle and aggregates these RMS values over defined intervals (e.g., 150/180 cycles, 10 sec, 10 min, 2 hr).

 

During an event, burst data logs the instantaneous voltage alongside the Vavg Sliding Ref Voltage. If the RMS voltage deviates from this baseline beyond configured thresholds (sag <90%, swell >110%), the event is flagged. The sliding reference ensures thresholds adapt to long-term changes in supply voltage, avoiding false positives.

 

For more information, please refer to standard IEC 61000-4-30 section 5.4.4 which pertains to the measurement methods for the duration of supply voltage dips and swells and defines the criteria for when an event begins and ends.

 

In the following technical note, you will find more information about the compliance of meters with the IEC 61000-4-30 (4-30) standard:
IEC 61000-4-30 compliance and ION meters

 

Best Regards,

-Mehran

L3 Expert Advanced metering

Reply
Dusica
Dusica
Contributor

Posted: ‎2025-12-24 02:58 AM

0 Likes
1
395
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
‎2025-12-24 02:58 AM

Hello Mehran, 


Thank you for your reply. In the standard IEC 61000-4-30:2015 Testing and measurement techniques there is formula to calculate sliding reference voltage as first-order filter (alpha=0.9967) with a 1-min time constant.

Is that the same formula Schneider uses to calculate "PQA1 Vavg Sliding Ref Voltage"?

 

Best regards, 
Dušica

Reply
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2026-01-02 08:34 AM

2 Likes
0
363
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
‎2026-01-02 08:34 AM

Hello @Dusica ,

 

Yes, the calculation is the same on the meter.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.