Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84606members
353882posts

PM8000 modbus register list ?

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
sesa38559
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
5
1180

PM8000 modbus register list ?


Hi Folks , am looking for a Modbus register listing for the PM8000 ?

Thanks 🙂


Accepted Solutions
ChenLiang
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: PM8000 modbus register list ?

Hi Pat O'Neill,

Please find it in the attachment.

See Answer In Context

Attachments
5 Replies 5
VictorMarincus
Sisko Sisko
Sisko

Re: PM8000 modbus register list ?

Hi Pat,

All the current documentation about PM8000 is available here (Documents & Downloads section):

http://www.schneider-electric.com/products/ww/en/4100-power-energy-monitoring-system/4112-intermedia...

You'll find the required document under the name of "PM8000 Modbus Map"

ChenLiang
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: PM8000 modbus register list ?

Hi Pat O'Neill,

Please find it in the attachment.

Attachments
sesa71269_bridg
Ensign Ensign
Ensign
0 Likes
2
919

Re: PM8000 modbus register list ?

Hello Guys,

This Modbus register list contains all registers and measured parameters?

Thanks, Laszlo

Hal_Etheridge
Janeway Janeway
Janeway

Re: PM8000 modbus register list ?

The ION devices have so many registers that it is impossible to expose them all through Modbus.  The Modbus protocol can only expose 64k 16 bit values - just about all the ION devices have at least 50k+ registers possible (and most of those are 32 bit integers or floating point values).

The core power metering registers are exposed by default and then additional registers can selectively be exposed by changing the device configuration to match your application.  If you want to take full advantage of the ION device capabilities you need to use the Power Monitor Expert or Power SCADA packages.

sesa56307_bridg
Lieutenant JG Lieutenant JG
Lieutenant JG

Re: PM8000 modbus register list ?

In ION meters other than the PM8000, it is true that the number of measurements mapped into Modbus is somewhat limited.  But to be clear, a major effort was made on the PM8000 to make all of the real-time measurements from the default ION template available in the Modbus map.  This does not mean providing every ION register as a Modbus register (since many of the ION modules/registers are interim values in the calculation chain and are not relevant measurements themselves).  Please refer to the published PM8000 Modbus map, and if you discover relevant real-time measurements for your application that are not listed, please let us know.

When creating new measurements through customizations to the ION framework, there is a limited capability to map these new values into Modbus using the Modbus Slave Modules in the ION framework.  Please also note that functions beyond reading real-time measurements are still limited today via Modbus (historical data, configuration, etc).