Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84257members
353362posts

PM8000 - TDD output source

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

skkim_isama_net
Lieutenant | EcoXpert Master Lieutenant | EcoXpert Master
Lieutenant | EcoXpert Master
0 Likes
1
195

PM8000 - TDD output source

Hello! PM Meter Team

basic Question

I needs PM8240 Tdd data, where can I found output module in the designer?

Tags (1)
1 Reply 1
Jose_Moreno
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: PM8000 - TDD output source

Hi ! kim seong-geun​ ,

You can obtain TDD values from the Harmonic Measurement Modules.

For that, you need to:

- Set up the "Display Mode" as "Magnitude Outputs Displayed as Percentages".

- Set up the "THD Display Mode" as "Percentages"

- Link the "Max Demand" input to the source for the peak or maximum demand load current. The demand load current might be a fixed value (provided with an External Numeric Module or Arithmetic Module), or it could be a maximum value over a period of time, calculated with a Sliding Window Demand Module and a Maximum Module.

Under these conditions, the TDD would be the "Total HD" output in your Harmonic Measurement Module.