Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM8000 MAC Authentication Bypass Functionality

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • PM8000 MAC Authentication Bypass Functionality
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
571
Mehran_Mehrnia
Mehran_Mehrnia Champion
202
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
Nicholas_Brown
Nicholas_Brown Explorer
Explorer

Posted: ‎2025-02-06 09:40 AM

0 Likes
1
919
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
‎2025-02-06 09:40 AM

PM8000 MAC Authentication Bypass Functionality

I have a customer that is attempting to connect a PM8000 (FW 4.5) to their network using IPv6 DHCP.  The meter is configured to do such.  The issue is that they are showing that the meter does NOT seem to be broadcasting it's MAC address via ARP.  They can see something connected to the port, but no MAC address.  They test this during a power cycle and when unplugging and re-plugging the Ethernet cable.

 

There are other PM8000s on different network segments (FW 3.1) that seem to be operating correctly and it is assumed they were able to broadcast their MAC address.  I don't have any other details on these.

 

Is there any potential that the FW versions may alter this behavior, or has anyone run into this issue of a PM8000 not broadcasting its MAC address for IPv6 DHCP?

 

Thank you.

Labels
  • Labels:
  • PM8000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-02-06 03:56 PM

0 Likes
0
886
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
‎2025-02-06 03:56 PM

Hello @Nicholas_Brown 

Firmware does not change the meter's ARP behavior. A meter with V4.5.0 that I tested with direct  connection had ARP message that included the meter's IPV4 address. With DHCP enabled, you see see a message from the meter requesting IPV6 IP address, subnet and gateway information after a power up. 

The devil in the details could be that the meter does not send out additional ARP messages after meter is powered on. There are ways to make the meter send out messages with the meter's MAC address. One way to do this is to have the meter modbus master a non existent IP address outside the subnet range. When meter tried to connect, will send a message out that includes the meter's MAC address. This works for IPv6 address, not sure if this would also work with IPV6.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Reply 1
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-02-06 03:56 PM

0 Likes
0
887
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
‎2025-02-06 03:56 PM

Hello @Nicholas_Brown 

Firmware does not change the meter's ARP behavior. A meter with V4.5.0 that I tested with direct  connection had ARP message that included the meter's IPV4 address. With DHCP enabled, you see see a message from the meter requesting IPV6 IP address, subnet and gateway information after a power up. 

The devil in the details could be that the meter does not send out additional ARP messages after meter is powered on. There are ways to make the meter send out messages with the meter's MAC address. One way to do this is to have the meter modbus master a non existent IP address outside the subnet range. When meter tried to connect, will send a message out that includes the meter's MAC address. This works for IPv6 address, not sure if this would also work with IPV6.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.