Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

PM8 Firmware

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • PM8 Firmware
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
581
Mehran_Mehrnia
Mehran_Mehrnia Champion
216
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
Ramon_Delgado
Ramon_Delgado Leader
Leader

Posted: ‎2014-05-29 07:02 AM

0 Likes
6
2107
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
‎2014-05-29 07:02 AM

PM8 Firmware

I heard that we are in the process of releasing new firmware for the PM8 meter, is there an ETA and where will the download be.  Can we get a pre-release firmware release notes?

Tags (2)
  • Tags:
  • firmware
  • pm8
Reply
  • All forum topics
  • Previous Topic
  • Next Topic
Replies 6
Anonymous user
Not applicable

Posted: ‎2014-06-02 12:31 PM

0 Likes
1
1979
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
‎2014-06-02 12:31 PM

The PM8 is in the process of releasing V12.5 which incorporates changes made in 12.4 (never commercially released) and 12.5. 

Reply
Hal_Etheridge
Hal_Etheridge Champion
Champion

Posted: ‎2014-06-02 01:04 PM

0 Likes
0
1979
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
‎2014-06-02 01:04 PM

Feature list or a list of the changes made?  Would be helpful to know so we can update the PME device driver (if needed) before customers let us know that things are broken. 🙂

Reply
Anonymous user
Not applicable

Posted: ‎2014-06-02 02:17 PM

0 Likes
3
1979
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
‎2014-06-02 02:17 PM

The firmware is already on the website available for download.  It incorporates V12.4 and 12.5

http://www.powerlogic.com/downloaddetail.cfm/cs/1/csec/2/fk_cat_id/1/fk_subcat_id/4/fk_p_id/17/fk_dc...

The website will have the release notes uploaded as well as a history pdf document.  Until we can get them up there here is a sneak peek:

V12.4 Changes

New Features:

- none

 

Modified Features:

- Added new registers 635, 636 and 637.

- You must enter the setup mode Command 9020 to be able to change registers 622 to 633 and registers 636 and 637. Command 9021 must be executed to save the changes made above.

- Added registers for tracking IP Address changes.

 

Bug Fixes:

- IP Address registers are now R/CW – Read / Conditional Write register.

- You must enter the setup mode Command 9020 to be able to change registers 622 to 633

- Added NOT_VALID_BYTE for I/O option module state initialization

- Fix to initialize I/O module correctly

12.5 Changes

New Features:

- none

 

Modified Features:

- If the S1 Input is set to Time Stamp NO 10 msec denouncing of the input will occur, this is done to allow for more accurate input time stamping.

- If the S1 Input is NOT SET to Time Stamp the 10 msec denouncing of the input will occur.

 

Bug Fixes:

Modified F/W to make the Time Stamp Accuracy to be within +- 4ms

Reply
Anonymous user
Not applicable

Posted: ‎2014-06-02 03:00 PM

0 Likes
0
1979
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
‎2014-06-02 03:00 PM

Here is a link with all the files:

http://www.schneider-electric.com/download/ww/en/details/470939524-PM800-Series-V125-Firmware/?showA...

Reply
Ramon_Delgado
Ramon_Delgado Leader
Leader

Posted: ‎2014-06-03 05:45 AM

0 Likes
1
1979
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
‎2014-06-03 05:45 AM

There is an error in the release notes regarding the commands to enter setup mode.  You have to enter 9020 to register 8000 to enter the setup mode, make the needed register writes to registers 622 to 633 and registers 636 and 637, enter 1 to register 8001 to save the entries and then 9021 to exit setup mode.  I just noticed that in the download that is on the Web site there is PM8_OS_12_500.fw, PM8_OS_12_510.fw, PM8_OS_12_520.fw so which one should be used?

Reply
Anonymous user
Not applicable

Posted: ‎2014-06-12 09:14 AM

0 Likes
0
1979
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
‎2014-06-12 09:14 AM

Thanks for letting us know.  We have corrected the website, to only include the 12.5 firmware, which can be downloaded at one of the two links above.
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.