Welcome to the new Schneider Electric Community

It's your place to connect with experts and peers, get continuous support, and share knowledge.

Close
Important Announcement: WELCOME to the Schneider Electric Community! We have moved to a new address: community.se.com — bookmark it today and contact SchneiderCommunity.Support@se.com if you have any questions!
Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
82754members
350542posts

PM5600 comm error

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

joel_mora_soati
Lieutenant
Lieutenant
0 Likes
1
210

PM5600 comm error

Hello Experts,

A customer reported a communication problem with a PM5650 after an interruption.

The meter is displaying 255.255.255.255 values.

I can enter the configuration and try to make the changes but as soon as I clic ok (individually) after modifying, the 255.255.255.255 value still present.

I notice with the QR code and meter insights platform that the value changed before is reflected in the IP value (via meter insights).

I try to make a point to point conection using the IP but the device is not reachable. Any thoughts about this behavior?

Tags (1)
1 Reply 1
Charles_Murison
Picard Picard
Picard
0 Likes
0
190

Re: PM5600 comm error

Hello @joel_mora_soati ,

 

Strongly recommend you contact technical support to start a case. (se.com -> support -> contact support). Be sure to include as much detail as possible including when this started, if you remember what the IP address was before. troubleshooting steps taken, firmware versions etc.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Tags (1)