Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84783members
354228posts

PM5350 Cannot save the clock time and can't be started after power cycle

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

sesa74337_bridg
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
2
431

PM5350 Cannot save the clock time and can't be started after power cycle

Dear Sir/Madam,

I have several PM5350 Power meters at a customer site, the clock just stays at 00:00:00, it never increases. If I put a time and hit save, the value will not be saved and the clock time just shown 00:00:00. The worst thing is, if I do a Power Cycle to the meter, the meter couldn't be started up, it shows "Schneider Electric" on the front display and blinking regularly. I would like to know if this is the known issue and how can I fix it?

It's not all the meters have such strange problem, I have recorded some of the meters Serial Numbers and OS

50139020

50139030

50139098

50139100

Date of Manufacture are all 17/02/13

OS Version: 1.11.1

RS version should be 1.0.0.0

Thank you so much,

Regards,

James Rong

Attachments
2 Replies 2
Charles_Murison
Picard Picard
Picard
0 Likes
1
361

Re: PM5350 Cannot save the clock time and can't be started after power cycle

If this is a matter of urgency please use Tech support to ask the question. This forum has no expectation of solving all questions.

L4 Prime for Advanced metering and Utilities
sesa74337_bridg
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
360

Re: PM5350 Cannot save the clock time and can't be started after power cycle

Hi, Charles,

Understand, I have raised this to Level 3. At the same time, if anyone has seen this before, please let me know. Thanks,

Cheers,

James