Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Ion 9000 is showing double the amount of VARs compared to other metering in the substation.

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • Ion 9000 is showing double the amount of VARs compared to other metering in the substation.
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
571
Mehran_Mehrnia
Mehran_Mehrnia Champion
203
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
sesa4025_bridge
sesa4025_bridge Explorer
Explorer

Posted: ‎2025-08-04 08:37 AM

0 Likes
1
573
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
‎2025-08-04 08:37 AM

Ion 9000 is showing double the amount of VARs compared to other metering in the substation.

We have looked at the phasor diagram and can see what the meter is seeing.  Everything appears to be in phase.  The issue is that the Ion 9000 is showing double the amount of VARs compared to other metering in the substation.  I know this has been an issue before, I had found a thread online discussing this very issue where they had to add a “triangulation module” to change the way the meter calculated the data.  Are you familiar with that at all?  It appears we are experiencing that same problem, and I am assuming it has to do with the CT circuits being wired in a delta configuration.

 

 I have an ION 9000 power quality meter at my company’s Park Substation location. We have noticed that the meter is reading VARS and Watts incorrectly compared to our Bitronics meters. We think the magnitude of the voltage
and current being read by the meter is correct, as the total VA match the Bitronics. For example, right now it is reading Vll avg of 12, 646 V, an I average of 478 A, a Vln average of 7,305 V, 6,734 kW, 8,134 kVARs, and 10,341 kVA. Our Bitronics are currently
reading 9.9 MW, 3.7 MVARs, and an I average of 485 A (These were all instantaneous values that are bouncing around a bit as I read them). We think the problem may be that the CTs for the meter are wired in delta, and we have not found an option in the configuration
to specify this. Since the CTs are wired in delta to get the current magnitude of 478 A we set the CT’s primary value to 692.82 which is 1200 / √3. The PTs are in wye, and there is a setting in the configuration to specify this. It appears if we could offset
each phase’s current by +30 degrees it would fix our problem. Is there a way to do this? Or, is there another solution to our problem?

Attachments
Labels
  • Labels:
  • ION9000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-08-04 10:44 PM

0 Likes
0
556
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
‎2025-08-04 10:44 PM

Hello @sesa4025_bridge 

 

Do you have a  wiring diagram of how the meter is connected to the system? 

 

I will start by saying I am a bit confused. The screenshot is from a meter that is not ION9000 based on the serial number. The values for voltage and current do not match your description.

When ION meters are showing kW that does not meet expectations when voltage and current magnitudes are at expected values, the most common issue is incorrect wiring. 

Also I am confused what you mean with changing the CT primary value. The setting on the meter should be matching the physical CT.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities

See Answer In Context

Reply
Reply 1
Charles_Murison
Charles_Murison Champion
Champion

Posted: ‎2025-08-04 10:44 PM

0 Likes
0
557
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
‎2025-08-04 10:44 PM

Hello @sesa4025_bridge 

 

Do you have a  wiring diagram of how the meter is connected to the system? 

 

I will start by saying I am a bit confused. The screenshot is from a meter that is not ION9000 based on the serial number. The values for voltage and current do not match your description.

When ION meters are showing kW that does not meet expectations when voltage and current magnitudes are at expected values, the most common issue is incorrect wiring. 

Also I am confused what you mean with changing the CT primary value. The setting on the meter should be matching the physical CT.

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.