Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84276members
353386posts

Information about MTR1-96

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
sesa213753
Schneider Alumni (Retired)
Schneider Alumni (Retired)
0 Likes
1
308

Information about MTR1-96

An Electrical Utility just added a line to the specification about

COMPLY WITH -> THE MTR1-96 CONSTRUCTION FOR POLYPHASE SOLID STATE ELECTRICITY METERS.

I was searching on google, and it seems that in our ION patents we mention this standard.

And this is my question, actually this is an standard? do we have some information about this ?

Markus Hirschbold

John Straughn

Alfredo Campozano

Sussex Davis

Attachments
Tags (3)

Accepted Solutions
sesa56425
Crewman Crewman
Crewman

Re: Information about MTR1-96

MTR1-96 is California ISO Engineering Specification for Poly-phase Solid-State Electricity Meters for Use on the ISO Grid. As far as I know the only certified meter is the ION8650.

https://www.caiso.com/Documents/ApprovedISOMeters.pdf

Regards,

Piotr.

See Answer In Context

1 Reply 1
sesa56425
Crewman Crewman
Crewman

Re: Information about MTR1-96

MTR1-96 is California ISO Engineering Specification for Poly-phase Solid-State Electricity Meters for Use on the ISO Grid. As far as I know the only certified meter is the ION8650.

https://www.caiso.com/Documents/ApprovedISOMeters.pdf

Regards,

Piotr.