Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84475members
353693posts

IPv6 Support by Schneider Devices

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

sesa82206
Schneider Alumni (Retired)
Schneider Alumni (Retired)

IPv6 Support by Schneider Devices


Team,

I was asked by a customer what are "Schneider's plans to support ipv6 in the future? Along with the power meters they  would also need to know the plans to support it on the protection meters eg micom,sepam, micrologics, etc.

I was advised that PM8000 supports IPv6 for local addressing, but how about the rest?

Regards,

3 Replies 3
ram_kaushik
Admiral Admiral
Admiral

Re: IPv6 Support by Schneider Devices

Received another enquiry from a customer on IPv6 support. The point to note is that this request is coming typically from IT network/security folks who are upgrading network infrastructure. We may see this hard-spec'ed very soon and we will have to demonstrate end-to-end support of IPV6 with all devices and software - not just isolated device support. This is one of those IT compatiblity items (like SSO or AD support) that could hurt us by completely blocking proposals. - please note for backlog!

Tom_Stevenson
Picard Picard
Picard

Re: IPv6 Support by Schneider Devices

Thanks Ram - I think a lot of us received the question today

We have had this on our backlog for a while and we have been monitoring the device support topic in order to pick our timing.

Thanks for the heads up

Tom

DanL
Commander Commander
Commander

Re: IPv6 Support by Schneider Devices

Just to clarify, the requirement for the PM8000 was to support link-local IPv6 for DPWS and HTTP only.