Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

ION9000 SubSynchronous Oscillation mapping

Metering & Power Quality

Schneider Electric support forum about Power Meters (ION, PowerTag, PowerLogic) and Power Quality from design, implementation to troubleshooting and more.
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
  • EcoStruxure Power & Grid
  • Metering & Power Quality
  • ION9000 SubSynchronous Oscillation mapping
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Charles_Murison
Charles_Murison Champion
575
Mehran_Mehrnia
Mehran_Mehrnia Champion
214
Ramasamy_N
Ramasamy_N Champion
115
View All

Recommended Forums

  • SmartConnector Forum

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Solved Go to Solution
Back to Metering & Power Quality
Start a Topic
Solved
SESA161069_EF33
SESA161069_EF33 Troubleshooter
Troubleshooter

Posted: ‎2026-09-17 05:29 AM

0 Likes
2
108
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
‎2026-09-17 05:29 AM

ION9000 SubSynchronous Oscillation mapping

Hello,

 

in ION9000, can the SubSynchronous Oscillation detection signal be mapped on an IEC61860 Goose signal or on a IEC61850 MMS signal ?
If not, on which communication protocol can it be mapped ?

In addition, where are accessible the IEC61850 PICS, MICS, PIXIT, TICS file ?

 

Best regards

Eric FIERFOL
Energy Business Automation COE
Lattes France
Labels
  • Labels:
  • ION9000
Tags (1)
  • Tags:
  • english
Reply
  • All forum topics
  • Previous Topic
  • Next Topic

Accepted Solutions
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2026-09-17 08:13 AM . Last Modified: ‎2026-09-17 08:14 AM

2 Likes
1
99
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
‎2026-09-17 08:13 AM

Hi @SESA161069_EF33 

 

The ION9000 does not support IEC 61850 GOOSE messaging, so the Subsynchronous Oscillation (SSO) detection/status signal cannot be published as a GOOSE message.

 

The ION9000 does, however, support IEC 61850 client/server communication as an IEC 61850 IED/server. This communication uses MMS (Manufacturing Message Specification) for client/server data exchange.

 

SSO information that is available as an ION register can potentially be exposed through IEC 61850 using the meter's custom GGIO modules, depending on the type of SSO output required:

  • Numeric SSO values can be mapped through the IEC 61850 GGIO Custom Analog module, which allows up to 16 user-selected numeric ION registers to be made available as IEC 61850 analog values.
  • Boolean SSO detection/alarm signals, if available or created as Boolean ION registers, can be mapped through the IEC 61850 GGIO Custom Digital module, which supports up to 16 Boolean ION registers.


The resulting communication path would therefore be:

SSO ION register → IEC 61850 GGIO → IEC 61850 client/server (MMS) → SCADA/IEC 61850 client

 

If IEC 61850 is not the desired method, Modbus TCP and DNP3 are also supported alternatives on the ION9000.

 

For DNP3, the ION9000 operates as a DNP slave/outstation, and its DNP map can be customized. The DNP Slave Export module can map an ION register to a DNP point for retrieval by a DNP master. Numeric values can be exposed as DNP Analog Inputs, while Boolean values can be exposed as Binary Inputs.

 

Therefore, the available approaches are:

  • IEC 61850 GOOSE: Not supported
  • IEC 61850 client/server (MMS): Supported, with custom GGIO mapping available
  • DNP3: Supported, with configurable ION-to-DNP mapping
  • Modbus TCP: Supported, with configurable mapping


Regarding the IEC 61850 PICS, MICS, PIXIT and TICS files, for the ION meters such as ION9000, IEC 61850 configuration and implementation information is provided primarily through the IEC 61850 and ION Technology documentation, the ION Reference, and the applicable ICD/CID files for implementation and configuration information.

 

The ION9000 firmware package provides the applicable ICD file, which is used with CET850 to build the CID file that is loaded into the meter to enable IEC 61850 functionality.

 

Best Regards,

-Mehran
L3 Expert Advanced metering

See Answer In Context

Reply
Replies 2
Mehran_Mehrnia
Mehran_Mehrnia Champion
Champion

Posted: ‎2026-09-17 08:13 AM . Last Modified: ‎2026-09-17 08:14 AM

2 Likes
1
100
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
‎2026-09-17 08:13 AM

Hi @SESA161069_EF33 

 

The ION9000 does not support IEC 61850 GOOSE messaging, so the Subsynchronous Oscillation (SSO) detection/status signal cannot be published as a GOOSE message.

 

The ION9000 does, however, support IEC 61850 client/server communication as an IEC 61850 IED/server. This communication uses MMS (Manufacturing Message Specification) for client/server data exchange.

 

SSO information that is available as an ION register can potentially be exposed through IEC 61850 using the meter's custom GGIO modules, depending on the type of SSO output required:

  • Numeric SSO values can be mapped through the IEC 61850 GGIO Custom Analog module, which allows up to 16 user-selected numeric ION registers to be made available as IEC 61850 analog values.
  • Boolean SSO detection/alarm signals, if available or created as Boolean ION registers, can be mapped through the IEC 61850 GGIO Custom Digital module, which supports up to 16 Boolean ION registers.


The resulting communication path would therefore be:

SSO ION register → IEC 61850 GGIO → IEC 61850 client/server (MMS) → SCADA/IEC 61850 client

 

If IEC 61850 is not the desired method, Modbus TCP and DNP3 are also supported alternatives on the ION9000.

 

For DNP3, the ION9000 operates as a DNP slave/outstation, and its DNP map can be customized. The DNP Slave Export module can map an ION register to a DNP point for retrieval by a DNP master. Numeric values can be exposed as DNP Analog Inputs, while Boolean values can be exposed as Binary Inputs.

 

Therefore, the available approaches are:

  • IEC 61850 GOOSE: Not supported
  • IEC 61850 client/server (MMS): Supported, with custom GGIO mapping available
  • DNP3: Supported, with configurable ION-to-DNP mapping
  • Modbus TCP: Supported, with configurable mapping


Regarding the IEC 61850 PICS, MICS, PIXIT and TICS files, for the ION meters such as ION9000, IEC 61850 configuration and implementation information is provided primarily through the IEC 61850 and ION Technology documentation, the ION Reference, and the applicable ICD/CID files for implementation and configuration information.

 

The ION9000 firmware package provides the applicable ICD file, which is used with CET850 to build the CID file that is loaded into the meter to enable IEC 61850 functionality.

 

Best Regards,

-Mehran
L3 Expert Advanced metering

Reply
SESA161069_EF33
SESA161069_EF33 Troubleshooter
Troubleshooter

Posted: ‎2026-09-18 01:37 AM

0 Likes
0
81
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
‎2026-09-18 01:37 AM

Thanks Mehran 

 

very clear.

Eric FIERFOL
Energy Business Automation COE
Lattes France
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.